2025-03-17 6:59 PM
Hi
When I try to set DSI clock more than 500M, the STM32cubemx will display an error message "dsi clock source frequency must be =< 62MHz" as below. But it said STM32H747 DSI clcok can reach 1Ghz in datasheet.
I use 25Mhz HSE and attach STM32cubemx project for reference.
2025-03-17 7:39 PM
Because it's the data across multiple lanes that can get to 1 Gbps
2-Lanes, clocking at 500 MHz each, the DSI clock on the wire is 250 MHz, with data lanes clocking on BOTH edges
The 62 MHz is the pixel clock, for a 16 or 24-bit load, the LTDC delivers words to the DSI, the DSI moves it a bit/lane over the wire.
16 x 62 = 992 bps
I suspect 16 x 62.5 = 1000 bps is the functional limit, or close too it.
The 24-bit colour depth the maximum pixel clock is closer to 41.67 MHz
If you don't like the limits the auto-gen tools apply, stop using them, and use your interpretation of the reference manual and the peripheral mechanics.
https://www.st.com/resource/en/product_training/STM32L4Plus_Peripheral_DSIHOST.pdf
2025-03-17 8:00 PM
This is the input clock to the DSI, not the speed of the output which is much higher.
@Tesla DeLorean explains it nicely here:
STM32H7 MIPI DSI maximum clock speed? - STMicroelectronics Community
2025-03-17 8:09 PM
Hi Tesla:
Thank you for your reply.
>Because it's the data across multiple lanes that can get to 1 Gbps
-->but as showing datasheet DS12930(https://www.st.com/content/ccc/resource/technical/document/datasheet/group3/99/a2/f9/3c/27/bc/48/a8/DM00602212/files/DM00602212.pdf/jcr:content/translations/en.DM00602212.pdf), per lane speed can reach 1 Gbps, not multiple lanes.
>I suspect 16 x 62.5 = 1000 bps is the functional limit, or close too it.
-->I think it would be better if it was officially confirmed, so let's wait for ST's answer.
>If you don't like the limits the auto-gen tools apply, stop using them, and use your interpretation of the reference manual and the peripheral mechanics.
-->The cubemx can save many time when starting a new project, I am just confused with this limitation.
2025-03-17 8:25 PM
Hi TDK:
It says 1 Ghz max here, so I think it still has something wrong here.
And in thread you mention, the VCO 2000 is red, but now it is't
2025-03-18 6:25 PM
Hi @mƎALLEm :
Can you help confirm this question?
2025-03-19 1:38 AM - edited 2025-03-19 1:39 AM
It will be handled by CubeMx team.
2025-03-20 5:43 PM
Hi @mƎALLEm :
Any update?
2025-03-24 2:55 AM
Hi @Souhaib MAZHOUD :
Can you help confirm this question?
2025-03-25 3:30 AM
Hello @Zhou JianQiang
This issue has been raised to the concerned team for review (Internal ticket number: 206060). I will get back to you as soon as I have any updates.
KR,
Souhaib