Yes, pin capacitance will vary per package, QFP has higher pin capacitance than BGA.from experience, I agree that "pin capacitance should be in range of 2pF to 3pF in general, in our datasheet we are providing worst case typical condition of 5pF ( ge...
some comments:0) check and ensure schematics/PCB/component are aligned.1) it is not good to probe at OSC pins, PH0/PH1, as crystal oscillation may be impacted. It is recommended to probe at MCO pin, PA8, by enabling MCO output from source = HSE after...
32768Hz jitter is common and normal, while 32768Hz clock long term stability is good in general.I suppose the "pll lock problem of MAX30001" is not directly link to 32768Hz jitter with STM32U585 or other MCU.
Your question:We would like to have a USB device with MSC only.Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 eval kit)? I think it is OK to have a USB device with MSC to work with...