2024-09-19 05:05 AM - edited 2024-09-19 05:06 AM
My setup is macOS 15.0 Sequoia
STM32CubeIDE 1.16.1
STLink-Server v2.1.1
When trying to program or debug a device the following error is shown:
Even after re-installing ST-Link server
I have rebooted and re-installed ST-Link Server, but the issue persists.
It's not a show stopper as I can use STM32CubeProgrammer to program the device, on the same machine.
Solved! Go to Solution.
2024-09-25 02:02 AM - edited 2024-09-25 02:03 AM
@pdmazariegos Thanks for the link to that solution on stackoverflow.
I find that it does indeed work. It's a better workaround than the one I came up with!
Hopefully the dev's at ST will be able to get to the bottom of it and push out a compatibiliy release in the near future. I have to keep my macOS up to date for other reasons, so I had no choice but to update to macOS 15.0
@SofLit Do you know if ST run a beta programme? I'd be happy to help with beta testing.
*edit* Spelling.
2024-09-28 01:36 AM
another one with the same problem:
2024-11-05
01:40 AM
- last edited on
2024-11-05
02:47 AM
by
Maxime_MARCHETT