STM32CubeProgrammer (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeProgrammer 2.17.0 released

STM32CubeProgrammer v2.17.0 release information New features:• Added the support for the STM32MP25xx microprocessors in the STM32MP2 series – Flash memory and OTP programming, SSP support Added the support for devices in the STM32WB0 series: STM32WB0...

CubeProgrammer shows that partition size is negative, fail to program using CubeProgrammer (kernel panic), but successful with raw SD card image using Win32DiskImager

Hi everyone,I have a problem using STM32CubeProgrammer (and CLI). They are both showing that my userfs partition have a size of -1162381824 bytes. That partition have size of 2.9GB. After programming with CubeProgrammer I have kernel panic, and I don...

0693W000007ZBa9QAG.png
NGajic by Associate III
  • 483 Views
  • 6 replies
  • 0 kudos

Resolved! What is the layout of the .tsv file?

I'm updating a .tsv file, used by the CubeProgramer to program a STM32MP DK1. The file I'm looking at contains:#Opt Id Name Type IP Offset Binary - 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-serialboot.stm32 - 0x03 ssbl...

MWors.1 by Associate II
  • 788 Views
  • 3 replies
  • 0 kudos

Resolved! Programming on board eMMC using Cube Programmer

Hi, We have a custom board with onboard eMMC which is connected on SDMMC2 lines: SDMMC2_D0 - PB14 SDMMC2_D1 - PB15 SDMMC2_D2 - PB3 SDMMC2_D3 - PB4 SDMMC2_D4 - PB8 SDMMC2_D5 - PB9 SDMMC2_D6 - PC6 SDMMC2_D7 - PC7 SDMMC2_CMD - PG6 SDMMC2_CLK - PE3 These...

NGajic by Associate III
  • 803 Views
  • 5 replies
  • 0 kudos

Resolved! Flashing STM32MP1 custom board over JTAG

Hello,I need to flash a custom STM32MP1 board which only has JTAG (no USB port available). Additionally, I build the image using Yocto meaning the output are separate binaries (e.g. U-Boot) and .tsv files.The STM32CubeProgrammer detects the CPU with ...

ANiko.3 by Associate II
  • 1440 Views
  • 12 replies
  • 0 kudos