STM32CubeProgrammer (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeProgrammer 2.17.0 released

STM32CubeProgrammer v2.17.0 release information New features:• Added the support for the STM32MP25xx microprocessors in the STM32MP2 series – Flash memory and OTP programming, SSP support Added the support for devices in the STM32WB0 series: STM32WB0...

Resolved! Using STM32CubeProgrammer (v2.2.0) to program SD card of our board (the board is base on STM32MP157C-DK2) but fail and get error message Error: Start operation failed at partition 0x01 Error: TSV flashing service failed

Hi,Our board is base on STM32MP157C-DK2 and the HW difference are...1. DK2 CN7 USB Type-C is replaced by micro USB and removed STUSB1600.2. DK2 CN6 PWR-IN is replaced by DC jack and CC1 is 0.4v to PA4 and CC2 keep 0v to PA5.And we would like to progr...

fctu by Associate II
  • 1863 Views
  • 4 replies
  • 0 kudos

How to solve this error? ===== DFU Interface ===== STM32_Programmer_CLI: symbol lookup error: STM32_Programmer_CLI: undefined symbol: libusb_get_port_number

I can't connect to my STM32MP157 evalaution board. I have installed required libraries as decribed in the tutorial: https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package 5.1 Installing the STM32CubeProgrammer tool. However I g...

KZura by Associate
  • 686 Views
  • 4 replies
  • 0 kudos

STM32CubeProg ubuntu 18.04 Failed to Parse

SEVERE: Failed to parse: /home/ubuntu/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.4.0/bin/libstp11_SAM.so.confHi, I'm trying to install STM32Cube on ubuntu 18.04 and it gives me error below, Please help me I'm struggling with this error f...

0693W000000W3GpQAK.png 0693W000000W3GkQAK.png 0693W000000W3GfQAK.png
ARehm by Associate III
  • 381 Views
  • 2 replies
  • 0 kudos