cancel
Showing results for 
Search instead for 
Did you mean: 

Verification progress bar bugged?

jefflongo
Associate III

When using the command line version of STM32CubeProgrammer, I notice during the verification process (-v flag), the progress bar follows a sequence like 6%->12%->18%->24%-18%->24%... and ends at 24%, with a successful verification. Picture provided for clarity. I am using STM32L021F4 and STM32CubeProgrammer version 2.3.0.0690X00000Bw3eTQAR.png

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @jefflongo​ ,

Well, the problem is still being analyzed and not fix it for 2.4.0 ,sorry for the delay 

I will give you an update as soon as possible.

Best Regards,

Khouloud

View solution in original post

13 REPLIES 13

Yes

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee

Hello @jefflongo​ ,

Thank you for highlighting the issue.

This is raised internally to the appropriate team for analysis and taking the necessary action.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Khouloud ZEMMELI
ST Employee

​Hello @jefflongo​  could you please share your .bin file ?

Thanks,

Khouloud

It won't let me directly upload a .bin file here so here is a link to the file. https://drive.google.com/open?id=1n2rCVDJbXuzldvBVJdc3xlPtuQ_NqnkI

​on my side it works fine , so could you please give me the log contents with Verbosity level 3?

Thanks,

Khouloud

@Khouloud ZEMMELI​ Here is the output. Thanks for continuing to look into this.

​Seems ok from your log file.

So from which tool you launched the CLI ?

Best Regards,

Khouloud

I'm running it from Git Bash terminal on Windows using the command​

STM32_programmer_cli.exe -c port=COM6 -w stm32dev.bin 0x08000000 -v -vb 3

Although I have tried several other terminals with similar results. I've also tried running it on a Linux machine with the same result.

​Issue reproduced, @jefflongo​  it will be fixed in the next release.

Best Regards,

Khouloud