cancel
Showing results for 
Search instead for 
Did you mean: 

Verification progress bar bugged?

jefflongo
Associate III

When using the command line version of STM32CubeProgrammer, I notice during the verification process (-v flag), the progress bar follows a sequence like 6%->12%->18%->24%-18%->24%... and ends at 24%, with a successful verification. Picture provided for clarity. I am using STM32L021F4 and STM32CubeProgrammer version 2.3.0.0690X00000Bw3eTQAR.png

13 REPLIES 13

Thank you!​

I updated to the new version 2.4.0, but the issue does not seem to be fixed. Any idea what's going on?

jefflongo
Associate III

@Khouloud ZEMMELI Could I get an update on this? Version 2.4.0 did not resolve the problem.

Hello @jefflongo​ ,

Well, the problem is still being analyzed and not fix it for 2.4.0 ,sorry for the delay 

I will give you an update as soon as possible.

Best Regards,

Khouloud