‎2020-11-25 12:04 AM
Hello,
I'm learning STM32 and wrote an quadspi external loader for my NUCLEO -144 (STM32743ZI) and 1M external flash. I've it tested in the Cube IDE and everything looks OK, I can read and write the external flash. When I use the loader in STM32CudeProgrammer I managed to read , but not erase and write accordingly. Any help will be appreciated. Please find attachments.
Thanks
‎2020-12-02 6:43 AM
cVass.1,
I just try to understand.. You managed read\erase\write an external flash by using STM32Cubeprogrammer and your custom external Quadspi loader (stldr) based on the project I sent you 4 days ago. Is it correct?
clive1
I get an error when trying to erase a sector of the external nor flash. Error: Sector erase operation has failed at least for one of the existing specified sectors.Please verify flash memory protection (shown on the picture) . I have EnableMemoryMappedMode enabled in my Init() of Loader_Scr.c
Does it make the problem? Have you idea?
Thanks
‎2020-12-02 8:05 AM
YGU.1
no this is my project, I just compare with mine.
during my tests I noticed that I was in EnableMemoryMappedMode in the Init (); I couldn't erase anymore.
‎2020-12-02 8:06 AM
I've been complaining about this for over a year
The initial load fails, the connect/disconnect/connect gets it right the second time around.
The ELF loader needs fixing if you're going to modify the addresses passed in the damn header and symbols. They'd actually work properly if left alone.
@STOne-32​
‎2020-12-02 8:15 AM
If you're in memory-mapped the erase probably will fail with HAL libraries.
Validate all code outside of the External Loader model first. Build a test harness so you can sequence the functions as Cube Programmer would so you can utilize a debugger.
You can always instrument your code to understand what it is doing, how Cube Programmer is interacting with it, and the errors you encounter on the HAL side. The USART and all your board hardware is available and can be used.
You can't really use interrupts, although I've seen some awful hacks from ST to get the HAL internal dependencies to work, you really don't need that for HAL_Delay and Ticks to work.
@STOne-32​ we really need to get some of this code on GitHub so we can fix the broken issues with Cube Programmer and ST-LINK Utilities that have persisted for years, and been ignored despite clear evidence of coding issues and initialization problems.
‎2020-12-02 10:09 AM
indeed I have the same concern as you.
I saw your other post.
18:57:48:223 : STLinkUSBDriver.dll loaded
18:57:48:224 : STLinkUSBDriver.dll loaded
18:57:48:225 : ST-LINK SN : 48FF6E068278535310410181
18:57:48:225 : ST-LINK FW : V2J37S7
18:57:48:226 : Board : --
18:57:48:226 : Voltage : 2.73V
18:57:48:233 : SWD freq : 4000 KHz
18:57:48:233 : Connect mode: Normal
18:57:48:233 : Reset mode : Software reset
18:57:48:237 : Device ID : 0x450
18:57:48:243 : Revision ID : Rev Y
18:57:48:278 : Buffer program...
18:57:48:278 : w ap 0 @0x580244F4 0x00000004 bytes Data 0x00000002
18:57:48:278 : Reading data...
18:57:48:278 : r ap 0 @0x58000528 0x00000004 bytes Data 0x00000001
18:57:48:279 : Buffer program...
18:57:48:279 : w ap 0 @0x580244F4 0x00000004 bytes Data 0x00000002
18:57:48:279 : Reading data...
18:57:48:280 : r ap 0 @0x58000528 0x00000004 bytes Data 0x00000001
18:57:48:280 : Buffer program...
18:57:48:281 : w ap 0 @0x580244F4 0x00000004 bytes Data 0x00000002
18:57:48:282 : Reading data...
18:57:48:283 : r ap 0 @0x58000528 0x00000004 bytes Data 0x00000001
18:57:48:283 : Buffer program...
18:57:48:283 : w ap 0 @0x580244F4 0x00000004 bytes Data 0x00000002
18:57:48:284 : Reading data...
18:57:48:284 : r ap 0 @0x58000528 0x00000004 bytes Data 0x00000001
18:57:48:285 : Reading data...
18:57:48:285 : r ap 0 @0x1FF1E880 0x00000004 bytes Data 0x00000800
18:57:48:285 : Database: Config 3 is active.
18:57:48:293 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x450.stldr is loaded
18:57:48:297 : Reading data...
18:57:48:297 : r ap 0 @0x1FF1E880 0x00000004 bytes Data 0x00000800
18:57:48:459 : UPLOADING OPTION BYTES DATA ...
18:57:48:459 : Bank : 0x00
18:57:48:459 : Address : 0x5200201c
18:57:48:459 : Size : 308 Bytes
18:57:48:460 : Reading data...
18:57:48:460 : r ap 0 @0x5200201C 0x00000134 bytes Data 0x0BD6AAF0
18:57:48:460 : UPLOADING OPTION BYTES DATA ...
18:57:48:460 : Bank : 0x00
18:57:48:461 : Address : 0x5200201c
18:57:48:461 : Size : 308 Bytes
18:57:48:461 : Reading data...
18:57:48:461 : r ap 0 @0x5200201C 0x00000134 bytes Data 0x0BD6AAF0
18:57:48:461 : UPLOADING ...
18:57:48:462 : Size : 1024 Bytes
18:57:48:462 : Address : 0x90000000
18:57:48:462 : Read progress:
18:57:48:462 : Reading data...
18:57:48:482 : halt ap 0 Status = 0
18:57:48:482 : halt ap 1 Status = 32
18:57:48:482 : halt ap 2 Status = 32
18:57:48:482 : w ap 0 reg 15 PC (0x24000000)
18:57:48:482 : w ap 0 reg 17 MSP (0x24000500)
18:57:48:483 : w ap 0 reg 16 xPSR (0x01000000)
18:57:48:483 : w ap 0 @0x24016F40 0x00000200 bytes Data 0x00000000
18:57:48:484 : w ap 0 @0x24000000 0x00000004 bytes Data 0x0000BE00
18:57:49:103 : w ap 0 @0x24000004 0x00016B08 bytes Data 0x00000000
18:57:49:103 : Init flashloader...
18:57:49:105 : halt ap 0
18:57:49:107 : w ap 0 reg 0 R0 0x00000000
18:57:49:107 : w ap 0 reg 1 R1 0x00000000
18:57:49:108 : w ap 0 reg 2 R2 0x00000000
18:57:49:108 : w ap 0 reg 3 R3 0x00000000
18:57:49:109 : w ap 0 reg 4 R4 0x00000000
18:57:49:109 : w ap 0 reg 5 R5 0x00000000
18:57:49:110 : w ap 0 reg 6 R6 0x00000000
18:57:49:110 : w ap 0 reg 7 R7 0x00000000
18:57:49:111 : w ap 0 reg 8 R8 0x00000000
18:57:49:112 : w ap 0 reg 9 R9 0x00000000
18:57:49:114 : w ap 0 reg 10 R10 0x00000000
18:57:49:114 : w ap 0 reg 11 R11 0x00000000
18:57:49:115 : w ap 0 reg 12 R12 0x00000000
18:57:49:116 : w ap 0 reg 13 SP 0x00000000
18:57:49:118 : w ap 0 reg 14 LR 0x24000001
18:57:49:118 : w ap 0 reg 15 PC 0x2000067D
18:57:49:119 : w ap 0 reg 16 xPSR 0x01000000
18:57:49:120 : w ap 0 reg 17 MSP 0x24016F08
18:57:49:120 : w ap 0 reg 18 PSP 0x00000000
18:57:49:121 : run ap 0
18:57:54:000 : halt ap 0
18:57:54:000 : Init function fail with timeout
18:57:54:001 : r ap 0 reg 16 xPSR 0x81000003
18:57:54:007 : halt ap 0 Status = 0
18:57:54:008 : halt ap 1 Status = 32
18:57:54:009 : halt ap 2 Status = 32
18:57:54:009 : w ap 0 reg 15 PC (0x24000000)
18:57:54:010 : w ap 0 reg 17 MSP (0x24000500)
18:57:54:011 : w ap 0 reg 16 xPSR (0x01000000)
18:57:54:012 : Error: Data read failed
‎2024-02-13 10:47 AM
I'm using a STM32H743 and I've tried to use your Loader_src.c, linker.ld, Dev_Inf.c/.h but get read error in programmer when I try to read the flash at 0x90000000. I've proven the quadspi.h and quadspi.c drivers for the Windbond W25Q64 work fine for Read, Write, and memory mapped. Any advice?
‎2024-02-14 5:05 AM
Have you mapped to your actual pins? Each Loader works for the chip but also for the pin distribution.
‎2024-02-14 6:50 AM
You're posting to a 3+ year old thread.
‎2024-02-14 12:56 PM
Yes, used the .ioc of the project to configure qspi so the drivers for qspi have the correct pin assignments. have a test in the code that writes a buffer to flash, reads flash, and enters memory mapped mode, all these tests passed just problem with .stldr used in programmer for some reason.
‎2024-02-14 1:16 PM
new thread on same topic...
Re: STM32H743 external loader - STMicroelectronics Community