2023-03-24 01:03 AM
Hello,
STM32CubeProgrammer 2.13 has some bugs:
Best regards,
Kraal
Solved! Go to Solution.
2023-05-31 04:41 AM
Hi @Aziz BRIGUI ,
Thank you for the feedback.
I have updated the best answer accordingly.
Best regards,
Kraal
2023-07-07 06:50 AM
Hello Aziz,
I've made the update to CubeProgrammer 2.14, from the release note it says that the 3 tickets are fixed.
However, regarding ticket number 149212 (Deselect all button in External Loaders tab), it is very strange. If I check the first one, Deselect all button is working (I mean that the external loader is unloaded AND the checkbox is unticked). Same for every other down to N25Q256A_STM32L476G_EVAL.
But if you select the very next one (N25Q256A_STM32L476G_EVAL_Cube) the button only unload the external loader, the checkbox stays ticked.
Of course my own loader is right after and shows the same issue with the checkbox.
However I have another loader at the end of the list, and this one works perfectly fine (unload and checkbox).
So I guess that this ticket 149212 will need some more love.
I still have to check the most important other point.
Best regards,
Kraal