2024-07-19 08:20 AM
Instead of completing development of STM32CUBE Programmer - every one now need to follow some manual steps with unknown versions of firmware with many undefined startup addresses and even when all steps are completed with success - development board still not programmed properly - examples are not working!!!
Solved! Go to Solution.
2024-07-21 07:17 PM
The error message come up when I am clicking the general link - Install updates - not related to any board.
2024-07-21 07:48 PM - edited 2024-07-21 07:48 PM
Ahh, so the Help -> Software Update? That doesn't work for me either. I get the same message you do.
You can download and install the newest version from the website. That'll do the same as the update.
STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics
Hope you figure it out. It can be frustrating. Cheers and good luck.
2024-07-22 08:30 AM
If people here are not developing STM32Cube software, nor are guiding development, or responsible for it - when all people here are wasting there time including me!