cancel
Showing results for 
Search instead for 
Did you mean: 

Program STM32G071 from Raspberry Pi

PNada.1
Associate II

Is it possible to program a STM32G071 from a raspberry pi running Raspbian OS? Is there a USB to serial driver for this?

3 REPLIES 3
TDK
Guru

If you're using an ST-Link to program, STM32CubeProgrammer should work on Linux.

If you're programming using the ROM UART bootloader, you'll need a usb to serial cable.

If you feel a post has answered your question, please click "Accept as Solution".
PNada.1
Associate II

So the linux installer is compatible with Raspbian OS? I saw there were two linux installers available-- Debian and generic linux. The SBC being considered is RPi 4. I will have to find out if the Debian installer will work on it.

Thank you,

Priya

I assumed Raspian was linux-based. Not that familiar with it.
If you feel a post has answered your question, please click "Accept as Solution".