2020-09-10 01:24 PM
Is it possible to program a STM32G071 from a raspberry pi running Raspbian OS? Is there a USB to serial driver for this?
2020-09-10 01:30 PM
If you're using an ST-Link to program, STM32CubeProgrammer should work on Linux.
If you're programming using the ROM UART bootloader, you'll need a usb to serial cable.
2020-09-10 02:51 PM
So the linux installer is compatible with Raspbian OS? I saw there were two linux installers available-- Debian and generic linux. The SBC being considered is RPi 4. I will have to find out if the Debian installer will work on it.
Thank you,
Priya
2020-09-10 03:01 PM