cancel
Showing results for 
Search instead for 
Did you mean: 

MKBOXPRO DFU Mode USB STM32CubeProgrammer

FilipeLourenço
Associate II

I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"

If anyone can help with this i appreciate.

I followed this instructions:

FilipeLoureno_0-1730132659258.png

5 REPLIES 5
FilipeLourenço
Associate II

I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"

If anyone can help with this i appreciate.

I followed this instructions:

FilipeLoureno_0-1730132659258.png

 

Andrew Neil
Super User

What Host system?

Does the system detect the unit?

eg, in Windows, does it appear in Device Manager?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Windows

It doesn't apear on the device manager.

Thanks!


@FilipeLourenço wrote:

It doesn't apear on the device manager.


Then, clearly, nothing on the system is going to be able to see it.

It's a basic connectivity issue - start with checking cables, etc.

Some suggestions here:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks!

The only thing that appears on my device manager is this: 

FilipeLoureno_0-1730899613641.png

Nothing that says STlink, but i am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, not using the STLINK V3 SET debbuger and programmmer.

The usb-C cable is the one from my new phone, that is a data cable too.

And i already tried all the usb ports.

 

Do you have any other reccomendations?

Shoud i buy the the STLINK V3 SET, debbuger and programmmer, to do the firmware update easier?