2024-10-28 09:27 AM - last edited on 2024-10-28 10:21 AM by Andrew Neil
I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"
If anyone can help with this i appreciate.
I followed this instructions:
2024-10-28 09:25 AM
I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"
If anyone can help with this i appreciate.
I followed this instructions:
2024-10-28 09:33 AM
What Host system?
Does the system detect the unit?
eg, in Windows, does it appear in Device Manager?
2024-10-29 02:21 AM
Windows
It doesn't apear on the device manager.
Thanks!
2024-10-29 02:34 AM
@FilipeLourenço wrote:It doesn't apear on the device manager.
Then, clearly, nothing on the system is going to be able to see it.
It's a basic connectivity issue - start with checking cables, etc.
Some suggestions here:
2024-11-06 05:42 AM
Thanks!
The only thing that appears on my device manager is this:
Nothing that says STlink, but i am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, not using the STLINK V3 SET debbuger and programmmer.
The usb-C cable is the one from my new phone, that is a data cable too.
And i already tried all the usb ports.
Do you have any other reccomendations?
Shoud i buy the the STLINK V3 SET, debbuger and programmmer, to do the firmware update easier?