cancel
Showing results for 
Search instead for 
Did you mean: 

MKBOXPRO DFU Mode USB STM32CubeProgrammer

FilipeLourenço
Associate II

I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"

If anyone can help with this i appreciate.

I followed this instructions:

FilipeLoureno_0-1730132659258.png

5 REPLIES 5
FilipeLourenço
Associate II

I am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, but the program doesn't detect any DFU port and gives the error : "Establishing connection with device failed"

If anyone can help with this i appreciate.

I followed this instructions:

FilipeLoureno_0-1730132659258.png

 

Andrew Neil
Evangelist III

What Host system?

Does the system detect the unit?

eg, in Windows, does it appear in Device Manager?

 

Windows

It doesn't apear on the device manager.

Thanks!


@FilipeLourenço wrote:

It doesn't apear on the device manager.


Then, clearly, nothing on the system is going to be able to see it.

It's a basic connectivity issue - start with checking cables, etc.

Some suggestions here:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

 

Thanks!

The only thing that appears on my device manager is this: 

FilipeLoureno_0-1730899613641.png

Nothing that says STlink, but i am trying to do the firmware upgrade via USB using STM32CubeProgrammer and putting the MKBOXPRO in DFU mode, not using the STLINK V3 SET debbuger and programmmer.

The usb-C cable is the one from my new phone, that is a data cable too.

And i already tried all the usb ports.

 

Do you have any other reccomendations?

Shoud i buy the the STLINK V3 SET, debbuger and programmmer, to do the firmware update easier?