cancel
Showing results for 
Search instead for 
Did you mean: 

Output log showing HWrst mode while it's connected over DFU mode

Rafa096
Associate II

I am building my own programmer app using the API provided with the CubeProgrammer program. If I follow the way I have to connect my board over DFU mode as in the USB_Example.cpp, this is the output:

STM32CubeProgrammer API v2.18.0 | Windows-64Bits

+++ USB Bootloader Example +++

------------- USB DFU List --------------
USB Port 0
USB index : USB1
USB SN : 3768346A3430
DFU version : 0x11A
-----------------------------------------

USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 DownLoad Firmware Update
SN : 3768346A3430
DFU protocol: 1.1
Board : --
IAP

--- Device Connected ---

while in the CubeProgrammer app, doing, I guess, exactly the same, this is the output:

Rafa096_0-1742370807022.png

It's showing the same output but with an extra line:

08:53:09: UR connection mode is defined with the HWrst reset mode

If I search in the cli documentation it says that this is reserved only for JTAG/SWD debug:

 -hardRst : Hardware reset
Available only with JTAG/SWD debug port

So why I am getting this line if I am connecting over DFU? and why is that line not showing in the output of the USB_example.cpp code?

Thanks

Rafa

1 ACCEPTED SOLUTION

Accepted Solutions
Amine_Jridi
ST Employee

Hello @Rafa096,

Thank you for bringing this to our attention. A ticket has been submitted to the development team for resolution.

Internal ticket number: 207264 (This is an internal tracking number and is not accessible or usable by customers).

Thanks,

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Amine_Jridi
ST Employee

Hello @Rafa096,

Thank you for bringing this to our attention. A ticket has been submitted to the development team for resolution.

Internal ticket number: 207264 (This is an internal tracking number and is not accessible or usable by customers).

Thanks,

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.