2023-12-28 08:01 AM - edited 2023-12-28 08:06 AM
I've got a brand new VM running Windows 11 pretty much off the shelf. I can install and run Cube IDE but when I try to install the STM32CubeProgrammer (64 bit version) I get into an infinite loop where the following happens:
- It opens the Install Wizard which then closes
- It opens the blue "STM32 Cube Programmer" window, which then closes
- It opens the Install Wizard which then closes
Here is a video of the behavior: https://www.loom.com/share/b3ce5e7a79ad425d840296845fd0c1ed
The only way I can exit this loop is to reset the whole machine. It's not installed, so I can't uninstall it. I tried removing everything, upgrading java, and still the same problem. Any suggestions would be appreciated. Thank you!
2023-12-28 09:14 AM
Hello @thayden and welcome to the ST Community
Can you try to install it with admin rights?
Best Regards.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-28 09:24 AM
Sadly the same problem! Here is a video link of me installing as administrator:
https://www.loom.com/share/c115cb558d004a33a49953e0a3b4bb0b
I hope this helps
2023-12-28 09:44 AM - edited 2023-12-28 09:46 AM
Great !
Exactly same endless movie, that it producing on my laptop on WIN10/64 , 22H2 .
I didnt complain about , because i think its almost useless, expecting a solution by STM.
STM has a new political orientation, now its most important to force users to login and check, whether there might be a cheap, old st-linkV2 and refuse working then to debug genuine STM cpus, than making programs, that work reliable or are at all working.
(btw in my case: End of "case" -> we cannot reproduce the error, so we cannot do anything about it. < )
2024-01-08 06:32 AM
Hello - just wondering if I can bump this thread for someone at ST to help. This is still an issue for me. Thank you!
2024-01-08 06:55 AM - edited 2024-01-08 06:56 AM
Hi,
You can call them for support :
and give a link to this thread .
2024-01-10 09:57 PM
Hello ST.. Any solution?
I'm having same issue, the GUI of STM32CubeProgrammer can't start.
2024-01-11 07:03 AM
Nope. I can't figure this out. Short of re-installing the entire OS, I'm not sure what to do..
2024-01-11 09:17 PM
I'm not sure if this information will help ST to figure out the problem.
Everything was working fine few months back with version 2.12.0.
Recently I saw latest version 1.15.0. I updated CubeProgrammer to this version.
Right after finished installation of 1.15.0, there's popup message saying I need to agree about sharing statistical data or something (not sure the exact words).
I click Ok button or agree button, but nothing happen. I have to force close using Windows task manager.
The next time I go into the CubeProgrammer, until now, the blue page shows for one second, then automatically closed.
2024-01-14 10:03 PM
I just found the workaround: Install 32bit version of STM32CubeProgrammer.
My laptop and the Windows OS is 64bit, so I normally install the 64bit version of STM32CubeProgrammer.
I don't feel difference using 32bit version. It does the basic job that I need (erase, download to MCU, verify).