cancel
Showing results for 
Search instead for 
Did you mean: 

Flash hex file to stm32f412 with uart using stm32cubeprogrammer

Vaishnavi
Associate II

Tried flashing stm32f412 custom controller using uart but facing error while going to boot mode.

I need to flash my hex file to custom stm32f412 board but unable to connect using uart and facing issue while erase memory

16 REPLIES 16

Better to open a new thread and share your schematics.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

@Vaishnavi wrote:

Can I flash my hex file with stlink 


Yes, of course that should work...

New thread on that:

https://community.st.com/t5/stm32cubeprogrammer-mcus/flash-hex-file-to-stm32f412-with-uart-or-stlink-using/m-p/729315

 

Hello

I'm using PA9-Tx and PA10-Rx for UART1 but couldn't able to flash

17:56:47 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

Hello @SofLit

I'm using PA9-Tx and PA10-Rx but facing issue while connecting 

11:12:47 : UR connection mode is defined with the HWrst reset mode
11:12:47 : RTS low
11:12:47 : DTR low
11:12:48 : Serial Port COM5 is successfully opened.
11:12:48 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
11:12:48 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again..

You've marked this as solved.

Are you now saying it is not solved?

BOOT0 pin? 

Lest' keep this thread closed as he's at first time using wrong UART pins.

Most probably the issue is on his HW. Keeping the discussion on this thread  by sharing the schematics.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.