cancel
Showing results for 
Search instead for 
Did you mean: 

Can't install V2.16.0 in Debian/Raspbian Linux - installer insta-quits

JU
Associate III

Per the title really - I've just tried to install the Linux version on a raspberry pi running Raspbian / Debian 11.7 'Bullseye' and, well, NOTHING happens.

If I click 'SetupSTM32CubeProgrammer-2.16.0.linux' nothing happens at all, if I select "execute in terminal" I get a brief flash of a terminal window, a mystery file of 0 bytes is created (named with a single unicode character and 'P').

If I run it from the terminal I get:

$ ./SetupSTM32CubeProgrammer-2.16.0.linux
-bash: ./SetupSTM32CubeProgrammer-2.16.0.linux: cannot execute binary file: Exec format error

 

 

Also why is a tool for programming microcontrollers a 286Mb download for which we must give ST our blood type and inside leg measurement just to be allowed to download it? :flushed_face:

1 REPLY 1
Maryem
ST Employee

Hello @JU ,

 

Currently STM32CubeProgrammer does not support ARM platforms. This request has already been raised to the development team. I will make sure to keep you informed of any advancements regarding this issue.

Internal ticket number: 162152 (This is an internal tracking number and is not accessible or usable by customers).

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.