2023-01-31 7:16 AM
I'm using NUCLEO-H755ZI-Q and I want to use USART3 on both M7 and M4 cores. The initializer is set to M7 as shown in the screenshot below. However, I can only get USART working on M7 but not on M4.
On the other hand, If I set the initializer to M4, then USART only works on M4 but not M7. It seems like HAL cannot work without an initializer. I would like to know the correct way to use HAL that can work on both cores. Thanks!
Solved! Go to Solution.
2023-02-01 8:05 AM
Hello @TKuo.1 ,
I think this thread may help you!
STM32 Dual Core using peripherals (UART) with both cores - best practice?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-01 8:05 AM
Hello @TKuo.1 ,
I think this thread may help you!
STM32 Dual Core using peripherals (UART) with both cores - best practice?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-02 6:16 AM
Thanks! I will take a look at it.