2020-01-14 01:18 AM
Upgraded STM32CubeMX from 5.4.0 to 5.5.0 and H7 firmware package to V1.6.0 and migrated.
When generating code it tells me the code is successfully generated but STM32CubeIDEproject generation have a problem.
Building the project fails:
make: *** No rule to make target 'C:/git/ELS/sbc_bootloader/CM7/Src/sys.c', needed by 'Application/User/sys.o'. Stop.
The same thing happens if I start a new project.
I'm using the STM32H745ZITx.
STM32CubeIDEproject generation have a problem, what problem?
Please fix 🙂
Solved! Go to Solution.
2020-01-15 03:02 AM
How did you get STM32CubeMX 5.5.0?. From complete fresh install or updating a 5.4.0 one ?.
If update could you have a try relying on your .ioc file AND complete 5.5.0 fresh install?
2020-01-14 01:41 AM
More info.
CubeMX is removing sys.c and sys.h files. Reverting them and I'm able to build the project. But not able to debug the project.
But I have a bad feeling about reverting to olde sys.c/h file. I'm guessing those files also have updates and that is why they are deleted but new files is not copied in.
2020-01-14 02:52 AM
Debug is working, my mistake not setting up for debug correctly.
So it seems like the missing sys.c/h file is the only issue.
Please fix 🙂
2020-01-14 09:01 AM
Any chance to share your .ioc file to get a try at ?
Code generation popup dialog you're getting sounds not so good ... some process is not able to end as expected most probably. May explain some issues then ...
2020-01-15 01:16 AM
Hello @Svenn Dahlstrom ,
Could you please share your ioc file and give more info about your machine and the java version ?
And it will be nice if you share your .log file.
Thanks,
Khouloud.
2020-01-15 01:35 AM
2020-01-15 01:44 AM
My machine is a Windows 10 1909
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) Client VM (build 25.231-b11, mixed mode)
Sorry, but I can't find any .log file in the project folder.
Or what file should I look for, and where?
2020-01-15 02:15 AM
.log under C:\Users\<user name>\.stm32cubemx, and please share your ioc file (generated with 5.4.0 cubemx version)
2020-01-15 02:38 AM
2020-01-15 02:40 AM