cancel
Showing results for 
Search instead for 
Did you mean: 

update issue, nothing works, it is not able to get into the internet connection

GKaja.1
Associate

i tried everything.

  • checked firewall
  • manually installed updates
2 REPLIES 2
S.Ma
Principal

I like the 18315 days since last update...

Let's radar sweep possible issues:

  • What is the CubeMX version?
  • There is a internet proxy setup page where communication can be tested OK or KO
  • Which country are you on?

Depending on the answers, full install CubeMX, cell phone tethering test or VPN might be worth trying.

5.5.0

i tried internet proxy, cell phone vpn, and the other stuff and it doesn't work, i even used manual and authentication type network in my workplace.

from India

totally unhappy for not being able to use stm on my laptop.

this is my system info in the pic attached..., I hope it helps