cancel
Showing results for 
Search instead for 
Did you mean: 

Clock configuration for Nucleo-H7A3

Marco.D
Associate II

Hello,

I started an empty project on CubeMX V5.5 (just updated) for a Nucleo-H7A3ZI,

I noticed that the clock default configuration for this board has a 64MHz clock.

If I change the multiplier on the PLL1 from x16 to x70 to get the max allowed 280MHz, I get an error on the 280MHz clock for AHB1,2 peripheral's clock.

However from the datasheet AHB clock can go up to 280MHz

Is this just a bug because this family has just appeared?

Regards,

Marco

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9

Hello @Community member​ 

Thanks for the feedback,

It will be fixed next CubeMX version.

Best regards,

Nesrine

Hi Nesrine,

thanks.

Something else that might also interest the community: is there a release date for it yet?

Thanks,

Marco

​next week.

Regards,

Nesrine

Marco.D
Associate II

Hi Nesrine

I've installed the new version, the CubeMX is able to configure the clocks for 280MHz,

however the code generated for the CubeIDE seems to had 2 bugs, can you please confirm:

Original code for SystemClock config:

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  LL_FLASH_SetLatency(FLASH_LATENCY_7);
 
  if(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_7)
  {
    Error_Handler();  
  }
  LL_PWR_ConfigSupply(LL_PWR_DIRECT_SMPS_SUPPLY);
  LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE0);
  LL_RCC_HSE_EnableBypass();
  LL_RCC_HSE_Enable();
 
   /* Wait till HSE is ready */
  while(LL_RCC_HSE_IsReady() != 1)
  {
    
  }
  LL_RCC_HSI48_Enable();
 
   /* Wait till HSI48 is ready */
  while(LL_RCC_HSI48_IsReady() != 1)
  {
    
  }
  LL_RCC_PLL_SetSource(LL_RCC_PLLSOURCE_HSE);
  LL_RCC_PLL1P_Enable();
  LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_8_16);
  LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
  LL_RCC_PLL1_SetM(1);
  LL_RCC_PLL1_SetN(70);
  LL_RCC_PLL1_SetP(2);
  LL_RCC_PLL1_SetQ(4);
  LL_RCC_PLL1_SetR(2);
  LL_RCC_PLL1_Enable();
 
   /* Wait till PLL is ready */
  while(LL_RCC_PLL1_IsReady() != 1)
  {
  };
 
   /* Intermediate AHB prescaler 2 when target frequency clock is higher than 80 MHz */
   LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
  
  LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);
  LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_1);
  LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_2);
  LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
  LL_RCC_SetAPB3Prescaler(LL_RCC_APB3_DIV_2);
  LL_RCC_SetAPB4Prescaler(LL_RCC_APB4_DIV_2);
  LL_SetSystemCoreClock(280000000);
 
   /* Update the time base */
  if (HAL_InitTick (TICK_INT_PRIORITY) != HAL_OK)
  {
    Error_Handler();  
  };
  LL_RCC_SetUSARTClockSource(LL_RCC_USART234578_CLKSOURCE_PCLK1);
  LL_RCC_SetUSBClockSource(LL_RCC_USB_CLKSOURCE_HSI48);
}

I think line 47 is wrong (SetAHBPrescaler is used in line 50), I believe it should be something like:

LL_RCC_SetSysPrescaler(LL_RCC_SYSCLK_DIV_1);

Also a line must be included to increase the programming delay (according to table 15 of the reference manual)

something like this after setting the latency (before line 13?):

 __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_3);   

Am I correct?

Thanks

Hello @Community member​ 

Could you please send me your .ioc file.

Regards,

Nesrine

Marco.D
Associate II

Here it is,

it has the default configurations, clock set for 280MHz plus a TMR1 configuration for pwm, nothing special.

Thanks,

Marco

Hi @Community member​ 

Function LL_RCC_SetAHBPrescaler cannot accept argument type LL_RCC_SYSCLK_DIV_2.

It should be LL_RCC_AHB_DIV_2.

For this line, __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_3); I will check it with the development team then i will tell you.

Regards,

Nesrine

Marco.D
Associate II

The clock is working ok because the AHBPrescaler is by default set to 1, however the programming delay is not set according to table 15, the (default) value for WRHIGHFREQ: Flash signal delay is 1 instead of 3.

Just a note: the previous version of CubeMX (5.5) was generating line 47 like this (which, as you say, would be wrong):

/* Intermediate AHB prescaler 2 when target frequency clock is higher than 80 MHz */
   LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_2);  

That is why I was suggesting to replace the LL_RCC_SetAHBPrescaler to LL_RCC_SetSysPrescaler.

I see now that the code divides the clock temporarily just before selecting the source for the sysclock, then it sets again the division to 1