cancel
Showing results for 
Search instead for 
Did you mean: 

To Generate 2 pwm with phase shift with same timers

vijay79444
Associate II

1000012502.jpg

 logic analyser picture has timer 1 channel 1 and another one is channel 2 it's duty 30% and frequency 100khz it's total ton+toff is 10 microseconds here I need to start the timer 1 channel 2 after 5 microseconds  I need the output like this I I'm drawn here

1000012503.jpg

 im using STM32H743IGT6 I had got the output in 50% duty but I can't get output other than 50% duty please help me anyone.

1 ACCEPTED SOLUTION

Accepted Solutions

>combined mode but that didn't work 

So you set it wrong .

read rm:

AScha3_0-1728640257525.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4

Use the Combined PWM mode.

JW

How can I do that I'm change pwm as combined mode but that didn't work 

>combined mode but that didn't work 

So you set it wrong .

read rm:

AScha3_0-1728640257525.png

 

If you feel a post has answered your question, please click "Accept as Solution".