2024-10-10 10:43 PM
logic analyser picture has timer 1 channel 1 and another one is channel 2 it's duty 30% and frequency 100khz it's total ton+toff is 10 microseconds here I need to start the timer 1 channel 2 after 5 microseconds I need the output like this I I'm drawn here
im using STM32H743IGT6 I had got the output in 50% duty but I can't get output other than 50% duty please help me anyone.
2024-10-11 12:17 AM
Use the Combined PWM mode.
JW