2023-06-19 12:06 PM
Hello guys, I'm currently working on a project with the STM32WL board, and using the LoRa application.
I'm having a problem with the RTC, what happens is that for the project I'm using the PingPong LoRa example, and I don't know exactly what is the internal configuration of it. For this reason, when I change the RTC mode from binary mode to BDC calendar and binary mode (because I need the date and time), the LoRa simply stops working, and I don't know why. Any ideia of what should I do?
2023-06-22 05:31 AM
Hello,
I can't reproduce the example this week, but I looked at the example code. My first guess is that you didn't changed the alarm settings, by masking the day/hours/minutes and seconds of the alarm. If you are still blocked I can give you more details next week when I got my hands on two WLs.
Have a nice one !
2023-08-16 11:51 AM
Hi, thanks for the reply. I tried chancing the alarm A settings, but I don't know what to change that'll make it work. Do you have any ideia?
2023-09-14 10:12 PM
2023-09-18 10:57 AM
Hello @Taksh,
I haven't solved it yet, still got the same problem, but for now I'm not giving too much of attention to the code.
If you eventually come across a solution feel free to leave it here!
2025-02-10 04:51 AM
Hi,
Has anyone found any solution for this? I also need to use the RTC in both binary and BCD modes for timestamps, but when I enable RTC_BINARY_MIX, LoRa stops working.
I’d appreciate it if you could share any progress or insights you’ve made on this issue.
Thanks in advance!
Best Regards,
Samidha