Hello Denys_T, Firstly, may I ask if you are using a Nucleo board ?If it's the case, I do think, it's normal cause PC13 is connected to the user button. You can remove SB51. You could try it routed to the second output, PB2, but I do think you need ...
Hello, Can you give me the code of the wakeup timer interruption and the rtc+wakeup intialization part ? In your program, does your wakeup timer trigger before you initialize the RTC (it shouldn't) ? I have a few possible ideas in mind. Thanks a lot ...
Hello, I don't know which code you are talking about but I was looking into one for bluetooth and it uses the wakeup timer (feature inside the RTC IP) for the timing which is independent of the date and time of the RTC (not 100% independant). Thus yo...