2019-05-17 5:56 AM
Is the FSMC_NL signal available on the PB7 pin in the LQFP64 housing? I am asking because STM32CubeMX does not have such a function for PB7 pin, and unfortunately I do not have time to test (I have to make a PCB for day before yesterday :( )
This function exists in STM32CubeMX, when LQFP100 body is chosen
2019-05-17 6:35 AM
IMO CubeMX is not an authoritative information source.
What does the datasheet say?
JW
2019-05-18 2:56 AM
Dear Waclawek.Jan, what do you think: why are there subsequent revisions of application notes ;)?
It's better and faster to ask. Maybe someone has a hardware experience (theory is actually in the application note).
The integrated circuit is't new and the STM32CubeMX is a ST branded tool.
Normally, I would test it myself or use the LQFP100, but it's chasing time and I do not have enough space on PCB.