2021-05-09 9:41 PM
Hello,
I am developing a board based on STM32F407G (Disc1) Where I am connecting an SD-Card over the SPI to store some data in the file on SD card. I am configuring internal RTC for the time tracking, On internal clock, a 16x2 LCD connected via 4-bit mode and some push buttons.
The problem I am facing is, When the Code do file operation on SD card(i.e writing data in file) the RTC time becomes 0. If board powered-up without the SD-card on it, It just works fine. For debugging I tried to do SD-Card activity after some time of booting(i.e. 30 Sec), So during the first 30 sec the RTC date-time showing fine, as the SD-Card operation started after 30 sec, RTC time-date became 0.
CubeMx configuration of the project is as below;
USART2(PD5, PD6)- asynchronous mode UART
SPI1(PB3-Clk, PB4-Miso, PB5-Mosi, PA15-GPIO_Out for CS)
PC0 to PC7-GPIO Output for LCD
PE0 to PE5-GPIO Input for Push-buttons
FATFS-User defined
RTC-Internal clock
TIM1-Micro second delay
For SD-Card configuration I followed: https://controllerstech.com/sd-card-using-spi-in-stm32/#:~:text=In%20this%20tutorial%20we%20will,writing%2C%20reading%2C%20deleting%20etc.
RTC: https://controllerstech.com/internal-rtc-in-stm32/
Can anyone please help me to understand what I missed here and resolve the issue? Also Let me know if anymore information required.
Thanks,
2021-06-01 7:05 AM
Hello @DParm.1 , can you please provide me with the IOC file to perform some analyzes ?
2021-06-02 1:55 AM
2021-06-03 3:21 AM
#MicroXplorer Configuration settings - do not modify
Mcu.Family=STM32F4
ProjectManager.MainLocation=Core/Src
FATFS._USE_FORWARD=1
PC7.GPIOParameters=GPIO_Label
USART2.IPParameters=VirtualMode
RCC.CortexFreq_Value=25000000
ProjectManager.KeepUserCode=true
Mcu.UserName=STM32F407VGTx
SPI1.VirtualType=VM_MASTER
TIM1.IPParameters=Prescaler
USART1.BaudRate=9600
RCC.PLLCLKFreq_Value=25000000
RCC.PLLQCLKFreq_Value=14285714.285714285
PC5.Locked=true
PC7.Locked=true
ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-false,3-MX_RTC_Init-RTC-false-HAL-true,4-MX_TIM1_Init-TIM1-false-HAL-true,5-MX_USART2_UART_Init-USART2-false-HAL-true,6-MX_SPI1_Init-SPI1-false-HAL-true,7-MX_FATFS_Init-FATFS-false-HAL-false,8-MX_USART1_UART_Init-USART1-false-HAL-true
PC0.GPIOParameters=GPIO_Label
PC0.GPIO_Label=RS
PC6.GPIO_Label=D6
VP_RTC_VS_RTC_Activate.Mode=RTC_Enabled
RTC.WeekDay=RTC_WEEKDAY_THURSDAY
RCC.RTCFreq_Value=32000
PD6.Locked=true
VP_RTC_VS_RTC_Calendar.Signal=RTC_VS_RTC_Calendar
USART1.IPParameters=VirtualMode,BaudRate
PC1.Locked=true
PinOutPanel.RotationAngle=0
RCC.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK
ProjectManager.StackSize=0x400
Mcu.IP4=SPI1
RCC.FCLKCortexFreq_Value=25000000
Mcu.IP5=SYS
NVIC.SVCall_IRQn=true\:0\:0\:false\:false\:true\:true\:false
Mcu.IP2=RCC
Mcu.IP3=RTC
Mcu.IP0=FATFS
Mcu.IP1=NVIC
TIM1.Prescaler=25-1
Mcu.UserConstants=
PC1.GPIOParameters=GPIO_Label
Mcu.ThirdPartyNb=0
SPI1.Direction=SPI_DIRECTION_2LINES
RCC.HCLKFreq_Value=25000000
Mcu.IPNb=9
RCC.I2SClocksFreq_Value=192000000
ProjectManager.PreviousToolchain=SW4STM32
RCC.APB2TimFreq_Value=25000000
PB6.Signal=USART1_TX
RCC.VcooutputI2S=192000000
PC7.Signal=GPIO_Output
PB6.Mode=Asynchronous
RTC.IPParameters=Hours,Minutes,WeekDay,Month,Date,Format
SPI1.CalculateBaudRate=48.828 KBits/s
Mcu.Pin6=PC2
Mcu.Pin7=PC4
Mcu.Pin8=PC5
PE5.Signal=GPIO_Input
Mcu.Pin9=PC6
PE1.Signal=GPIO_Input
RCC.AHBFreq_Value=25000000
Mcu.Pin0=PE2
PD5.Mode=Asynchronous
Mcu.Pin1=PE3
Mcu.Pin2=PE4
Mcu.Pin3=PE5
Mcu.Pin4=PC0
Mcu.Pin5=PC1
ProjectManager.ProjectBuild=false
RCC.HSE_VALUE=8000000
RTC.Minutes=59
NVIC.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:true\:false
NVIC.DebugMonitor_IRQn=true\:0\:0\:false\:false\:true\:true\:false
PB3.Mode=Full_Duplex_Master
NVIC.SysTick_IRQn=true\:0\:0\:false\:false\:true\:true\:true
ProjectManager.FirmwarePackage=STM32Cube FW_F4 V1.25.2
MxDb.Version=DB.6.0.0
RTC.Month=RTC_MONTH_DECEMBER
PB4.Mode=Full_Duplex_Master
ProjectManager.BackupPrevious=false
RCC.VCOInputFreq_Value=2000000
PC4.GPIO_Label=D4
PB5.Mode=Full_Duplex_Master
File.Version=6
PE3.Locked=true
PE2.Signal=GPIO_Input
PB7.Signal=USART1_RX
PE1.Locked=true
PB6.Locked=true
NVIC.PendSV_IRQn=true\:0\:0\:false\:false\:true\:true\:false
PE4.Signal=GPIO_Input
ProjectManager.HalAssertFull=false
VP_TIM1_VS_ClockSourceINT.Mode=Internal
ProjectManager.ProjectName=F4_UART
FATFS._USE_LABEL=1
RCC.MCO2PinFreq_Value=25000000
Mcu.Package=LQFP100
VP_FATFS_VS_Generic.Signal=FATFS_VS_Generic
USART2.VirtualMode=VM_ASYNC
ProjectManager.ToolChainLocation=
RCC.LSI_VALUE=32000
VP_SYS_VS_Systick.Signal=SYS_VS_Systick
VP_RTC_VS_RTC_Calendar.Mode=RTC_Calendar
PA15.Signal=GPIO_Output
RCC.APB2CLKDivider=RCC_HCLK_DIV2
RCC.APB1TimFreq_Value=12500000
NVIC.BusFault_IRQn=true\:0\:0\:false\:false\:true\:true\:false
PC4.Locked=true
PC5.Signal=GPIO_Output
PD6.Signal=USART2_RX
SPI1.BaudRatePrescaler=SPI_BAUDRATEPRESCALER_256
PD5.Locked=true
PC2.GPIO_Label=EN
ProjectManager.CustomerFirmwarePackage=
PC4.GPIOParameters=GPIO_Label
PB3.Locked=true
PB4.Signal=SPI1_MISO
VP_RTC_VS_RTC_Activate.Signal=RTC_VS_RTC_Activate
ProjectManager.ProjectFileName=F4_UART.ioc
Mcu.PinsNb=26
ProjectManager.NoMain=false
SPI1.IPParameters=VirtualType,Mode,Direction,CalculateBaudRate,BaudRatePrescaler
PC4.Signal=GPIO_Output
PC2.Signal=GPIO_Output
PC6.Signal=GPIO_Output
ProjectManager.DefaultFWLocation=true
PD5.Signal=USART2_TX
ProjectManager.DeletePrevious=true
PC0.Signal=GPIO_Output
RCC.APB1CLKDivider=RCC_HCLK_DIV4
boardIOC=true
PD6.Mode=Asynchronous
RCC.FamilyName=M
FATFS.IPParameters=_USE_CHMOD,_USE_LABEL,_USE_FORWARD
PA15.Locked=true
ProjectManager.TargetToolchain=SW4STM32
PC6.Locked=true
PC5.GPIOParameters=GPIO_Label
VP_TIM1_VS_ClockSourceINT.Signal=TIM1_VS_ClockSourceINT
PE4.Locked=true
PB5.Locked=true
RTC.Format=RTC_FORMAT_BIN
PC2.Locked=true
ProjectManager.RegisterCallBack=
PE0.Locked=true
RCC.LSE_VALUE=32768
VP_FATFS_VS_Generic.Mode=User_defined
RCC.VCOI2SOutputFreq_Value=384000000
board=STM32F407G-DISC1
RCC.VCOOutputFreq_Value=100000000
ProjectManager.LastFirmware=true
RCC.APB2Freq_Value=12500000
MxCube.Version=6.0.1
SPI1.Mode=SPI_MODE_MASTER
PC2.GPIOParameters=GPIO_Label
PC1.GPIO_Label=RW
VP_SYS_VS_Systick.Mode=SysTick
RCC.EthernetFreq_Value=25000000
NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:true\:false
PE5.Locked=true
ProjectManager.FreePins=false
RCC.IPParameters=48MHZClocksFreq_Value,AHBFreq_Value,APB1CLKDivider,APB1Freq_Value,APB1TimFreq_Value,APB2CLKDivider,APB2Freq_Value,APB2TimFreq_Value,CortexFreq_Value,EthernetFreq_Value,FCLKCortexFreq_Value,FamilyName,HCLKFreq_Value,HSE_VALUE,HSI_VALUE,I2SClocksFreq_Value,LSE_VALUE,LSI_VALUE,MCO2PinFreq_Value,PLLCLKFreq_Value,PLLM,PLLN,PLLP,PLLQ,PLLQCLKFreq_Value,RTCFreq_Value,RTCHSEDivFreq_Value,SYSCLKFreq_VALUE,SYSCLKSource,VCOI2SOutputFreq_Value,VCOInputFreq_Value,VCOOutputFreq_Value,VcooutputI2S
ProjectManager.AskForMigrate=true
Mcu.Name=STM32F407V(E-G)Tx
PE0.Signal=GPIO_Input
RCC.RTCHSEDivFreq_Value=4000000
Mcu.Pin24=VP_SYS_VS_Systick
ProjectManager.UnderRoot=true
Mcu.Pin25=VP_TIM1_VS_ClockSourceINT
Mcu.IP8=USART2
FATFS._USE_CHMOD=1
PC7.GPIO_Label=D7
Mcu.IP6=TIM1
Mcu.IP7=USART1
ProjectManager.CoupleFile=false
RCC.48MHZClocksFreq_Value=14285714.285714285
PB4.Locked=true
PB3.Signal=SPI1_SCK
RCC.SYSCLKFreq_VALUE=25000000
RTC.Hours=23
PB5.Signal=SPI1_MOSI
Mcu.Pin22=VP_RTC_VS_RTC_Activate
Mcu.Pin23=VP_RTC_VS_RTC_Calendar
Mcu.Pin20=PE1
Mcu.Pin21=VP_FATFS_VS_Generic
NVIC.ForceEnableDMAVector=true
KeepUserPlacement=false
PC5.GPIO_Label=D5
NVIC.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:true\:false
USART1.VirtualMode=VM_ASYNC
ProjectManager.CompilerOptimize=6
PB7.Mode=Asynchronous
ProjectManager.HeapSize=0x200
Mcu.Pin15=PB4
NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:true\:false
Mcu.Pin16=PB5
Mcu.Pin13=PD6
PC6.GPIOParameters=GPIO_Label
Mcu.Pin14=PB3
Mcu.Pin19=PE0
ProjectManager.ComputerToolchain=false
Mcu.Pin17=PB6
RCC.HSI_VALUE=16000000
Mcu.Pin18=PB7
RCC.PLLP=RCC_PLLP_DIV4
RCC.PLLQ=7
NVIC.PriorityGroup=NVIC_PRIORITYGROUP_0
Mcu.Pin11=PA15
Mcu.Pin12=PD5
RCC.PLLM=8
RCC.PLLN=50
Mcu.Pin10=PC7
PB7.Locked=true
PE2.Locked=true
PE3.Signal=GPIO_Input
RCC.APB1Freq_Value=6250000
RTC.Date=31
PC0.Locked=true
ProjectManager.DeviceId=STM32F407VGTx
PC1.Signal=GPIO_Output
ProjectManager.LibraryCopy=1
2021-06-03 3:41 AM
Read out and check/compare RTC and RCC_BDCR registers content between "working" and "non-working" case.
JW