cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F372/STM32F373 as a USB host

FLast.5
Associate II

When I was going through the setup process of USB in STMcubeMX, I suspected that it could not be used as USB host.

I would like to know if STM32F372/STM32F373 can be used as USB host. Can STM32F372/373 be used as USB host?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, the USB block in the STM32F373 can only work as a device and not as a USB host.

BTW: the STM32F372 was removed from the datasheet many years ago and has since become obsolete.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Correct, the USB block in the STM32F373 can only work as a device and not as a USB host.

BTW: the STM32F372 was removed from the datasheet many years ago and has since become obsolete.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FLast.5
Associate II

Yes. Thank you.

No.

JW