2022-03-09 06:13 PM
When I was going through the setup process of USB in STMcubeMX, I suspected that it could not be used as USB host.
I would like to know if STM32F372/STM32F373 can be used as USB host. Can STM32F372/373 be used as USB host?
Solved! Go to Solution.
2022-03-10 01:14 AM
Correct, the USB block in the STM32F373 can only work as a device and not as a USB host.
BTW: the STM32F372 was removed from the datasheet many years ago and has since become obsolete.
Does it answer your question?
Regards
/Peter
2022-03-10 01:14 AM
Correct, the USB block in the STM32F373 can only work as a device and not as a USB host.
BTW: the STM32F372 was removed from the datasheet many years ago and has since become obsolete.
Does it answer your question?
Regards
/Peter
2022-03-10 01:26 AM
Yes. Thank you.
2022-03-10 02:39 AM
No.
JW