2019-02-26 11:50 AM
I opened an older project which was created with 5.0.1, and the newest CubeMX shows an error for this option in ADC. But this option is correct. I tried to create a new project, and I wasn't able to enable this option here.
Solved! Go to Solution.
2019-11-02 08:19 PM
Hi,
I'm using CubeMX 5.4.0 with FW package from Sept 2019, and I still have this issue: I set the DMA to work in circular mode using simultaneous ADC1&2, this doesn't translate into the code, it still generates this way:
hadc1.Init.DMAContinuousRequests = DISABLE;
So DMACFG is 0 and I just get one round of conversion, once I reach the end of the buffer in which the DMA stores the data, it stops.
I edited the CubeMX in a text editor, it shows correctly Dma.ADC1.0.Mode=DMA_CIRCULAR, I expect this is what enables hadc1.Init.DMAContinuousRequests. It doesn't.
If I set DMACFG in the debugger manually then the circular mode works.
Ben.
2020-07-14 03:56 PM
2020-07-17 07:27 AM
Hi @JWhit.7 , I'll check it.
Regards,
Khouloud
2020-07-17 07:37 AM
you're right, the 6.0.0 will be available for the next week, it's OK on 6.0.0.
We are deeply sorry for any inconvenience this may have caused.
Regards,
Khouloud