2020-12-04 04:09 AM
Hello, i have found some bugs
I can't select the external 32 khz osc .
---
the input field of the User Label have some problems
edit this fields don't work properly
CTRL + c/v don’t work
Solved! Go to Solution.
2020-12-14 02:29 AM
Hi @Hans T
So to conclude, for the first problem related to LSE activation : you need to Enable RTC if you want to change RTC Clock Mux.
For the seconde one which is a problem with User Label, thanks for sharing your ioc file to reproduce the issue, you're right and it will be fixed.
Thanks for your feedback, please mark my answer as best if its answered your question, this will help other users find this solution more quickly..
Khouloud
2020-12-04 06:10 AM
Hi @Hans T
For the LSE Problem : you need to Enable RTC in you want to change RTC Clock Mux.
For the User Label and fields Problem : Can you please explain more what's exactly the issue, seems Ok.
For the CTRL+C Problem : You're right, the issue will be internally analyzed.. But can you please explain what does the CTRL+ V mean ?
Thanks for your feedback, Khouloud
2020-12-04 07:00 AM
Ctrl+C is copy. Ctrl+V is paste.
2020-12-04 07:16 AM
yes copy past
:thumbs_up:
2020-12-04 07:26 AM
->For the LSE Problem : you need to Enable RTC
yes, it works thanks
2020-12-04 07:48 AM
Thanks @TDK , @Hans T I thought you meant by Ctrl-C : Close Project as mentioned in UM.
So @Hans T can you please explain the issue with copy and past ? also the User Label and fields Problem?
Thanks, Khouloud
2020-12-04 09:18 AM
Enter User label in the Pinout view works good
only the UserLabel in the Configuration field is an problem
2020-12-07 12:14 AM
@Hans T ,
Please share your ioc file to check the problem, and can you specify where exactly the Problem ? ( Under which IP ? Pin name ? )
Your feedback on copy and paste will be important for me to help you solve this issue.
Thanks, Khouloud
2020-12-13 01:40 AM
I send you the IOC PM
2020-12-14 02:29 AM
Hi @Hans T
So to conclude, for the first problem related to LSE activation : you need to Enable RTC if you want to change RTC Clock Mux.
For the seconde one which is a problem with User Label, thanks for sharing your ioc file to reproduce the issue, you're right and it will be fixed.
Thanks for your feedback, please mark my answer as best if its answered your question, this will help other users find this solution more quickly..
Khouloud