STM32CubeMX v4.26 SD Card Problem Continues [STM32F4 Discovery]
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-19 05:21 AM
Hi,
I've been dealing with the SD card problem since the CubeMX version 4.
Here are the corresponding parts of my code:
...
...
...
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/ FATFS myFATFS = {0}; FIL myFILE; UINT testByte;/* USER CODE END PV */
...
...
...
/* USER CODE BEGIN 2 */
if(f_mount(&myFATFS, SDPath, 1) == FR_OK){ char myPath[] = 'WRITE1.TXT\0'; f_open(&myFILE, myPath, FA_WRITE | FA_OPEN_ALWAYS); char myData[] = 'Hello World\0'; f_write(&myFILE, myData, sizeof(myData), &testByte); f_close(&myFILE); HAL_Delay(1000); } /* USER CODE END 2 */...
...
...
Here, the problem is in f_mount, it doesn't go forward. Debugging further, the code stucks in 'ff.c' file at the following bold line (line 3050):
/* Find an FAT partition on the drive. Supports only generic partitioning rules, FDISK and SFD. */
bsect = 0;
fmt = check_fs(fs, bsect); /* Load sector 0 and check if it is an FAT-VBR as SFD */
if (fmt == 2 || (fmt < 2 && LD2PT(vol) != 0)) { /* Not an FAT-VBR or forced partition number */
for (i = 0; i < 4; i++) { /* Get partition offset */
pt = fs->win + (MBR_Table + i * SZ_PTE);
br[i] = pt[PTE_System] ? ld_dword(pt + PTE_StLba) : 0;
}
This problem continues in the last 4 version, and still not fixed. Can someone try to create a project from scratch with STM32CubeMX version 4.26 and FW F4 v1.21 which are both the lastest versions by the moment?
Here are few extra notes:
- I set minimum heap and stack size as 0x2000 and 0x4000.
- I'm using Keil uVision MDK v5.15 with compiler v5.05 update 2 (build 169).
- My operating system is Windows 7 Pro SP1 64 bits.
- I'm sure that there is no hardware issue as I was able to run the SD card with a example project.
Regards,
Ogulcan
#f_mount #stm32cube-fw_f4-v1.0 #cubemx-4.26 #fw_f4-v1.0 #sd-card #cubemx #stm32f4 #fatfs #sdcard-fatfs Note: this post was migrated and contained many threaded conversations, some content may be missing.- Labels:
-
FatFS
-
SDIO-SDMMC
-
STM32CubeMX
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-28 02:03 AM
Hello,
I also encountered issues with FATFS and SD-CARD a while ago. Code failed at fmount() and it was because SD-CARD was not initialised in SD_initialize() function.(Note: This function is genrated by Cube) I have attached the link to the issue below.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-11 02:00 AM
Please can you post the Image of other side of the sdcard board for Soldering reference .also please share the working code since i have been trying from past 3 weeks.(STM cubemx+Truestudio9.1)
Thank you
Ashwinraj
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-11 02:53 AM
Dear Ashwinraj,
Please refer to following URL and picture.
https://github.com/jason0627/STM32F4-Discovery_SDIO_4bit_OK
Best regards,
Jason
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-11 03:02 AM
Hi,
I've spent months on the issue and thanks to Jason, I've managed to make it work. I've found out that I actually need to set DMA and NVIC in the versions after 4.21, so I suggest you to look at the DMA and NVIC setttings.
Cheers,
Ogulcan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-12 02:41 AM
Thank you very much. but i figured out solution for few latest cubeMX4.26
1) Enable DMA
2) use 22 ohm series resistor
3) In cubemx change the application structure to Advanced(check attach image) or else in truestudio you will get path entry warning
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-03 01:43 AM
Dear Ashwinraj,
can you share complete project along with cubemx ioc file to understand it completely?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-04 03:27 PM
Hi,
My problem was slightly different. 1 bit mode with DMA worked but 4-Bit mode did not. In 4-Bit mode f_mount was hanging.
I'm using the STM32F769NI discovery board and the system clock needed to be higher than the SD card clock. Originally had SDMMC clock set to divider of 0 but it was flacky. Changed system clock to run faster than SDMMC clock and used PLL48MHz as input clock to SD module. After this change no problems with f_mount or reading or writing.

- « Previous
- Next »