2019-03-02 12:01 AM
I just designed a board with the new STM32F730Z8 value line with embedded USB high speed PHY. I'm using a 16MHz external crystal and I am using the default code generated with CubeMX. It fails in the USBD_Init function. Following it through at first glance I found that in usbd_conf.c there is this line:
hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_ULPI_PHY;I changed the interface to USB_OTG_HS_EMBEDDED_PHY but it still fails. I imagine there could be some other settings that may be wrong as well. Any guidance on this?
Solved! Go to Solution.
2019-03-04 8:44 AM
@Khouloud ZEMMELI
I confirmed there is a problem. I created a new project for the STM32F723ZE and it ran on the F730.
Diffing the files shows two places it is different, the first was the USB_OTG_HS_EMBEDDED_PHY as listed above, and it also included:
__HAL_RCC_OTGPHYC_CLK_ENABLE();in the HAL_PCD_MspInit function. Making those two changes allows the MX_USB_Init function to succeed. I can see the device connect to my computer but it has an error message. I think this particular problem is solved.
2019-03-04 2:32 AM
Hello @bobert
Thank you for the feedback.
Can you please share your ioc file ?
Regards,
Khouloud.
2019-03-04 3:32 AM
2019-03-04 8:44 AM
@Khouloud ZEMMELI
I confirmed there is a problem. I created a new project for the STM32F723ZE and it ran on the F730.
Diffing the files shows two places it is different, the first was the USB_OTG_HS_EMBEDDED_PHY as listed above, and it also included:
__HAL_RCC_OTGPHYC_CLK_ENABLE();in the HAL_PCD_MspInit function. Making those two changes allows the MX_USB_Init function to succeed. I can see the device connect to my computer but it has an error message. I think this particular problem is solved.