STM32CubeMX: STM32F413 assert on ADC_CHANNEL_TEMPSENSOR => Macro bug?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-17 7:22 AM
Hey guys,
i did setup my project using Cube MX, configured all outputs and inputs.
Generated the Startupcode with CubeMX.
Directly after start of main() MX_ADC1_Init() is called.
I did setup the Temp Sensor as well
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
sConfig.Rank = 11;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
However
assert_param(IS_ADC_CHANNEL(sConfig->Channel));
fails. So i was wondering. is there a Bug in the IS_ADC_CHANNEL Macro or am I missing something?
I'm using the latest HAL (STM32F4 Cube V1.24)
Labels:
- Labels:
-
ADC
-
Bug-report
-
STM32CubeMX
-
STM32F4 Series
0 REPLIES 0