2019-03-11 05:37 AM
I can't measure tempsensor with vbat and vref because cubemx generates low layer code in the following order:
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_6, LL_ADC_CHANNEL_TEMPSENSOR);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SAMPLINGTIME_640CYCLES_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SINGLE_ENDED);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR);
/** Configure Regular Channel
*/
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_7, LL_ADC_CHANNEL_VREFINT);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_VREFINT, LL_ADC_SAMPLINGTIME_640CYCLES_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_VREFINT, LL_ADC_SINGLE_ENDED);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_VREFINT); // Previously enabled tempsensor bit get overwritten here and only internal vrefint channel is enabled.. I took a few hours until I figured out why ny MCU temp measuring module isn't works since I ported my ADC to HAL from LL
Finaly result is only vrefint is enabled and tempsensor is disabled. CubeMX should use logical OR in this case. In HAL it is implemented correctly, but this implementation missing from LL.
Solution is:
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR | LL_ADC_PATH_INTERNAL_VREFINT);
2020-05-31 09:01 AM
Any news on this? I'm working with F4 now and it's also present here not only for L4.
2021-03-10 08:36 AM
Just wasted a few hours on this, so it STILL isn't fixed.
This (generated by CubeMX) does not work:
LL_ADC_REG_SetSequencerChAdd(ADC1, LL_ADC_CHANNEL_TEMPSENSOR);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR);
LL_ADC_REG_SetSequencerChAdd(ADC1, LL_ADC_CHANNEL_VREFINT);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_VREFINT);
But this does:
LL_ADC_REG_SetSequencerChAdd(ADC1, LL_ADC_CHANNEL_TEMPSENSOR);
LL_ADC_REG_SetSequencerChAdd(ADC1, LL_ADC_CHANNEL_VREFINT);
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR | LL_ADC_PATH_INTERNAL_VREFINT);
2022-06-07 05:02 AM
Any news on this? I'm working with the up-to-date framework / tools and still not fixed for F7.
(Same bug reported here: https://community.st.com/s/question/0D50X0000C20aDzSQI/bug-cubemx-550-stm32g0-wrong-setcommonpathinternalch-initialization )
Edit: On the F767xx this a bit more complicated. While chapters 15.10 and 15.11 of the reference manual (RM0410) state that only VBAT and internal temperature sensor can't be used at the same time.
Reality shows and register description of ADC_CCR state that VBAT can't be used with temperature sensor OR VREFINT at the same time.
I suggest a fix of the reference manual (update the chapter 15.11 note) and maybe a warning when generating invalid combinations with CubeMX.
2023-02-09 05:12 AM
@Khouloud ZEMMELI Any news on this ?? It's crazy that it has to take ST more than 4 years to correct such a simple bug like this... Very annoying for anybody during all this time who spend hours to understand what is wrong with your libraries, because someone doesn't want to correct it.
2023-02-16 12:58 AM
@Motla , First I want to apologize for the delay made to fix this issue, @Khouloud OTHMAN Could you please take in charge the follow up of that issue (or one of the support team) as I don't work on support anymore?
2025-01-27 01:38 PM
@Khouloud OTHMAN Any news ? Problems still exists. Still pending in CubeMX even in STM32H5xx.
2025-01-27 01:40 PM
CubeMX 6.9.2 with STM32H5xx
Error still exists. Wasted lots of hours to find out the error.
Vrefint and temp-sensor and VBat as ADC Channel in CubeMX activated.
even though the according Bits "VREFEN , TSEN, VBATEN in ADC_CCR are always not set. (Keil debugger)
By manualy activating these bits in the debugger everything works.
IIs there a chance to fix this problem in CUBE MX after 3 Years?
fortunately this helps:
LL_ADC_SetCommonPathInternalCh(__LL_ADC_COMMON_INSTANCE(ADC1), LL_ADC_PATH_INTERNAL_TEMPSENSOR | LL_ADC_PATH_INTERNAL_VREFINT);
Thanks Henry