2022-07-20 01:03 PM
I am using STM32CUBEMX 6.6.1. When trying to export a Kicad model, the model turns out empty without any Pins.
2022-07-21 04:44 AM
Welcome, @Christian Pommer, to the community!
How did you export a model from a project created using STM32CubeMX to import it into KiCAD?
Regards
/Peter
2022-07-22 12:46 PM
Hello Peter,
I used the TOOL -> CAD Tab.
Choosing Kicad as CAD Product. Export Pins including labels. Then download CAD Model.
The model is generated but includes no connectable pins as shown in the following graphic.
I also checked the generated files. It only contains the information for the shape.
Best regards,
Christian Pommer
2022-07-22 01:06 PM
You would have to explain in more detail how you exported this, CAD Tab is completely unknown to me at least.
2022-07-23 05:50 AM
The CAD Subtab was added with STM32CUBEMX 6.6 and can be found right below the PCC power tools in the tools tab.
Steps to reproduce:
I am sorry for not providing the necessary steps in the first place.
2022-07-23 05:10 PM
Indeed... Well, the point 4 is a good example how things can be hidden in plain sight!
2024-07-17 01:02 AM
Bug again occurs, please let me know when it is fixed.