2015-01-03 04:40 AM
I have STM32CubeMX v4.12, Check for Updates
revealed
STM32CubeF1 Release 1.3 After dondloadint , but Cube say: This Package version is not managed on this version of STM32CubeMX. Wher is probl�m?I am talking
about
#stm32cube #stm32cubemx #stm32f12016-01-04 02:53 AM
Hi Charles,
Could you please explain how you get the firmware update: is it automatically asked by MX or did you selected a local installation done manually?-Syrine-2016-01-04 09:14 AM
For the first time
offered
me the
MX
update
automatically
over Check update ManagerAfter the failure
, I
tried
and manual
installation.
For completeness
,
the MX
now
has
this update
no
offers
.2016-01-05 12:23 AM
Type text or a website address or
https://translate.google.cz/?tr=f&hl=en
https://translate.google.cz/?tr=t&hl=en
</div>Translate from:
Yesterday I
discovered the
STM32CubeF1 1.3
updates
on the second
PC.
Downloading and installing
OK
. In New Libraries Manager I see STM32Cube F1 Releases 1.2 and 1.3 too, all with green square as installed. After restarting STM32CubeMX, I see only version 1.2, Check Update Manager not offer any update. In folder Repository is folder STM32Cube_FW_F1_V1.2.0 and STM32Cube_FW_F1_V1.3.0 too. OS I have Windows 7 x64 on first PC and Windows 7 x86 on second PC, all updates Installed. Installation MX is standard only, installation folder changed from C:\.. to D:\.. and Repository Folder changed on D:\Program Files\STMicroelectronics\STM32Cube\Repository2016-01-10 03:33 AM
I today on new computer install last version of CubeMX 4.12.
Unfortunately,
it
also
offered as
the latest version
CubeF1
v 1.2Version
1.3
can not be installed
for manual
download from the
ST web page.2016-01-15 03:41 AM
Dear Sir/Madam,
I can confirm the issue as experienced on my PC. Latest STM32CubeMX has been installed (V4.12.0), Installation of STM32Cube_FW_F1_V1.3.0 from local download fails with error message: ''This Package version is not managed on this version of STM32CubeMX.'' Due to firewall restrictions, direct update download could not be tested. Best regards2016-01-20 02:56 AM
Hi,
The STM32CubeF1 Firmware Package V1.3.0 is now available for download using update interface of MX 4.12.-Syrine-