2023-05-10 7:08 PM - edited 2023-11-20 5:45 AM
Hi all,
I'm trying to use STM32CubeIDE to create a project for this board from the list of "Examples Selector". I picked "Demonstrations" as seen in the picture. I don't see a ".ioc" file and when I try to build I get these errors:
Description Resource Path Location Type
make: *** No rule to make target 'C:/Users/myUserName/STM32W/Demonstrations/STM32CubeIDE/Utilities/lcd/stm32_lcd.c', needed by 'Utilities/stm32_lcd.o'. Stop. Demonstrations_CM4 C/C++ Problem
make: *** No rule to make target 'C:/Users/myUserName/STM32W/Demonstrations/STM32CubeIDE/Utilities/lcd/stm32_lcd.c', needed by 'Utilities/stm32_lcd.o'. Stop. Demonstrations_CM7 C/C++ Problem
I tried 3 different projects and all 3 don't have the ".ioc" file. That's the file that shows the visual configurator pinout among other things. In a effort to find out more I picked a different board (NUCLEO-L476RG, example "GPO"). This time I get an ".ioc" file and the project builds without errors.
I'm new to STM32 and the whole ecosystem. The NUCLEO-H745ZI-Q is dual core, the NUCLEO-L476RG is single core. How do I get the dual core project to show the ".ioc" file ... and build without errors?
Thanks
Solved! Go to Solution.
2023-05-17 6:08 AM - edited 2023-11-20 5:46 AM
Hello @Rodo ,
To import the project in STM32CubeIDE1.12.0 version, I recommend you to follow these steps:
1- Open STM32CubeIDE1.12.0 version
2- Click File-->Open Projects from File System as shown in the below figure
3- Browse the Demonstrations\STM32CubeIDE project file located in this path "STM32Cube_FW_H7_V1.11.0\Projects\NUCLEO-H745ZI-Q\Demonstrations\STM32CubeIDE" as shown in the below figure
4-Build the Demonstrations_CM4 project as shown in the below figure
5-Build the Demonstrations_CM7 project
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-11 1:01 AM
Examples/Demonstrations have not ioc file. If you create project from scratch, use mcu selector or board selector. Example selector allows to choose project that has some code, readme and it's ready to flash on your board.
2023-05-11 9:32 AM
Are you saying "Examples/Demonstrations have not ioc file" for the NUCLEO-H745ZI-Q? The other board example I picked works fine. See bold font in my post. Thanks.
2023-05-15 8:39 AM
Hello @Rodo ,
Which STM32CubeIDE version are you using?
I made some tests using STM32CubeIDE.1.12.0 version and the STM32Cube_FW_H7_V1.11.0 firmware version and I didn't find any issue.
Please, try to use the last STM32CubeIDE version and let me know if the problem is solved.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-15 10:14 AM
I have STM32CubeIDE 1.12.0. I'm new to STM so I just installed it about a month ago. I don't know how to check "STM32Cube_FW_H7_V1.11.0 firmware". The picture I posted shows this version. I had a friend check this demo using his Linux machine and got the same error as me. There was no ioc file and he got the two make errors I showed in my post. I don't have the default workspace folder name though I changed it to "STM32W" maybe that makes a difference?
Is there a way for you to zip the project and post it here?
2023-05-15 10:21 AM
I just saw that exclamation symbol next to the name. I tried to make the project again and I notice a message related to that symbol in the upper left corner that says:
"Selected example is still in development and may not be fully functional"
I selected another demo (GPIO_EXTI) for the board and this one doesn't have a ioc file either but it builds without errors.
2023-05-16 4:57 AM
2023-05-16 10:51 AM - edited 2023-11-20 5:45 AM
How about instructions how to import this into cubeIDE? I tried to "import project" from the information center screen but what I got didn't work. Thanks:
2023-05-17 6:08 AM - edited 2023-11-20 5:46 AM
Hello @Rodo ,
To import the project in STM32CubeIDE1.12.0 version, I recommend you to follow these steps:
1- Open STM32CubeIDE1.12.0 version
2- Click File-->Open Projects from File System as shown in the below figure
3- Browse the Demonstrations\STM32CubeIDE project file located in this path "STM32Cube_FW_H7_V1.11.0\Projects\NUCLEO-H745ZI-Q\Demonstrations\STM32CubeIDE" as shown in the below figure
4-Build the Demonstrations_CM4 project as shown in the below figure
5-Build the Demonstrations_CM7 project
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-17 1:56 PM
Ok that built without errors. Thanks. Before I mark it as answered, one last thing ... there is still no ioc (visual configuration) file in the project. How do I get that? Thanks