2018-11-25 9:17 AM
I use the CubeMX command-line interface. Normally I put my script in a file, and run it like this:
java -jar "C:\path\to\STM32CubeMX.exe" -q "C:\path\to\myscript.txt"
But before doing that, I test the script commands one-by-one in the interactive mode. That means, I start up CubeMX with the command line interface and I can see visually what happens upon each command I enter:
java -jar "C:\path\to\STM32CubeMX.exe" -i
The first command I usually issue then is to load an existing `ioc-file`:
config load "C:\path\to\my_cubemx_proj.ioc"
Then I issue the following command:
set mode FREERTOS Enabled
This works. I can see immediately the green checkmark appearing next to `FREERTOS` in the Middleware section. The next thing I do is changing the Timebase Source in SYS from `SysTick` to `TIM1`:
set mode SYS TIM1 Timebase Source
This used to work in the previous CubeMX version. But in CubeMX5 it doesn't have any effect. The following image illustrates what happens:
Solved! Go to Solution.
2019-10-24 3:22 AM
Hi,
I discovered the answer (through trial and error).
set mode FREERTOS CMSIS_V1
set mode SYS TIM1
The main problem is this:
The CubeMX documentation explains how the `set mode` command works:
set mode <Periph> <Mode Name>
but nowhere can I find the values I should fill in for the placeholders.
2018-11-28 2:31 AM
Hi @Kristof Mulier ,
Thanks for rising this issue.
It will be fixed next CubeMX release.
Best regards,
Houda
2018-11-28 3:28 AM
Thank you @Houda GHABRI
I look forward to the new release. I've noticed that not only he `SYS` settings, but many other settings in CubeMX cannot be adapted anymore using the command line interface. Hopefully they'll get fixed as well.
I'm happy STMicro provides the CubeMX tool as a standalone application with both a Graphical User Interface and a command line interface. This one of the reasons I prefer using STMicro chips compared to other manufacturers. Nowadays, many manufacturers create their code generator tools as a mere plugin for Eclipse, without standalone version. That's really awful, because it forces people to use Eclipse.
Thumbs up for STMicro :)
2018-11-28 11:33 PM
Hi @Kristof Mulier ,
Thanks for being faithful TO ST products and appreciate them.
We try to improve continually CubeMX.
Please do not hesitate to rise any issue or remarks.
Best regards,
Houda
2018-11-29 1:06 AM
Hi @Houda GHABRI ,
Thank you for your reply.
I like the new "look and feel" of CubeMX V5. It is refreshing :)
2019-01-27 3:29 AM
Hi @Houda GHABRI ,
Can you please contact the development team of CubeMX for this issue? Our startup is creating a new product - based on STM32 microcontrollers - to be announced on the Nuremberg Embedded World conference (we rent a stand in the startup area). The issue described above is blocking our development. Please, please help...
2019-10-24 3:22 AM
Hi,
I discovered the answer (through trial and error).
set mode FREERTOS CMSIS_V1
set mode SYS TIM1
The main problem is this:
The CubeMX documentation explains how the `set mode` command works:
set mode <Periph> <Mode Name>
but nowhere can I find the values I should fill in for the placeholders.