2024-12-17 10:04 AM - edited 2024-12-17 10:11 AM
Folks,
I’m grappling with what looks like a low level bug** , and the root cause could be running out of stack space. At the same time, I’ve got plenty of unused RAM, so I’d like to increase the stack size as a diagnostic measure, and see if the bug goes away*** . In the CubeIDE user guide (UM2906) there’s a mention that heap and stack size are set in the LinkerScript.ld (comments in the code on p. 69).
If I want to change the _Min_Stack_Size , should I edit the LinkerScript.ld file directly?
Or is the LinkerScript.ld file (re)generated by the IDE, and I should make the change through the IDE GUI?
If so then where are these settings?
I couldn't figure it out from the UM2906. I saw hints that CubeMX had GUI fields settings for stack and heap.
** Can post the details of the bug if anyone’s interested.
*** Don’t know if that’s the right long-term solution. I could also try to declare fewer string buffers on the stack.
Best regards,
- Nick
2024-12-17 10:11 AM - edited 2024-12-17 10:13 AM
I understand the dilemma, the .LD impacts what the Linker actually builds, but ST for years has nailed the GNU/GCC stack to Top-of-Ram directly via _estack
And then used SP to provide a heap ceiling for _sbrk, ie from end-of-statics to base-of-stack
2024-12-19 01:02 AM - edited 2024-12-20 12:11 AM
Hello @Nick Alexeev
In order to change the _Min_Stack_Size and _Min_Heap_Size using GUI fields.
just go to Project manager -->project
Unfortunately, for the meantime, there is a limitation in this option that has been tracked with internal ticket 197963.
THX
Ghofrane
2024-12-19 02:34 AM
That doesn't answer the more general question about editing the .ld file.
How should that be managed - especially for things that are not provided in the MX GUI ?
2024-12-19 08:39 AM
An IDE bug is a serious matter. Where are the details of the IDE bug published? Post a link, please.