2021-05-20 1:26 AM
Hi, everyone!
I have a custom board with an STM32H7. I configured SDMMC2 correctly on it.
As you can see there is no options for configuring DMA since it has an Internal (I)DMA.
I have also added FATFS, as follows.
I managed to write/ready successfully to SD CARD mounted via FATFS. My problem arises when I enable the ‘Use DMA Template’. It is a must in order to later add FreeRTOS to the project.
After hours of debugging I realized that:
Any help is highly appreciate it :folded_hands: .
2021-05-20 4:32 AM
Hi @Mohammed Eshaq ,
Please make sure that you are not hitting one of the conditions that makes "DMA is not working on STM32H7 devices".
You can also refer to following example available under STM32CubeH7 package (path: Projects\STM32H743I-EVAL\Applications\FatFs\FatFs_uSD_DMA_RTOS).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-02 6:38 AM
Hi @Mohammed Eshaq ,
Were you able to solve the issue you described here? If yes it will be helpful for us and other Community members to know what was the solution?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-06 11:43 PM
Hi @Amel NASRI ,
I appreciate your follow-up. But, no, the solution provided did not solve my problem. I have tried the following.
I noticed that SDMMC2_IRQHandler() does get called but exits without calling BSP_SD_WriteCpltCallBack(). I get HAL_SD_ERROR_TX_UNDERRUN. I spent days debugging this and trying different configurations but with no luck!
2021-07-01 3:59 AM
Hi Sirlsaac,
I also have this problem. I solved it by:
/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
}
/* Define output sections */
SECTIONS
{
/* Stuff unchanged (FLASH initialization) here ... */
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM_D1 AT> FLASH /************ Replace here please ***********/
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM_D1 /************ Replace here please ***********/
/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM_D1 /************ Replace here please ***********/
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
void SDMMC1_IRQHandler(void)
{
/* USER CODE BEGIN SDMMC1_IRQn 0 */
/* USER CODE END SDMMC1_IRQn 0 */
//HAL_SD_IRQHandler(&hsd1);
BSP_SD_IRQHandler(0); /*************** Replace here ****************/
/* USER CODE BEGIN SDMMC1_IRQn 1 */
/* USER CODE END SDMMC1_IRQn 1 */
}
Hope it helpfull!
-Hai-