2020-05-12 11:14 AM
I already reported this bug up at previous versions of the STM32H7 firmware.
Now I'm using
For those who find SDMMC not working, there still is an obvious bug , the way the code is generated by STM32CubeMX. If we look at the below code:
void MX_SDMMC1_SD_Init(void)
{
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 2;
hsd1.Init.TranceiverPresent = SDMMC_TRANSCEIVER_NOT_PRESENT;
}
We seem to be missing a few lines in there.
EDIT: DTK mentioned this, because the Init code was missing the initialization functions, I also changed the bits to 8 because of thinking of eMMC I also use. But this was for SD-cards, where I use 4-bit sofar, a slip of the pen. Now Clive just did show that 8-bit SD-Cards also exist, so it still would be valid. In my working code, I did correct fine though, and it works, because after generation I always add and change things and don't let STM32CubeMX modify it anymore. Because not everywhere always are comment lines where I need to change things.
This is just about wondering why the generated code is missing the init function after filling the structure. The ioc file is below, maybe there is an error in there.
Now I need to test if STM32CubeMX always leaves the init function out, both for SD and MMC.
So now I added SD and MMC parts.
SD:
void MX_SDMMC1_SD_Init(void)
{
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 2;
hsd1.Init.TranceiverPresent = SDMMC_TRANSCEIVER_NOT_PRESENT;
if (HAL_SD_Init(&hsd1) != HAL_OK)
{
Error_Handler();
}
}
MMC:
void MX_SDMMC1_MMC_Init(void)
{
hmmc1.Instance = SDMMC1;
hmmc1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hmmc1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_ENABLE;
hmmc1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hmmc1.Init.BusWide = SDMMC_BUS_WIDE_8B;
hmmc1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_ENABLE;
hmmc1.Init.ClockDiv = 0;
if (HAL_MMC_Init(&hmmc1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
I hope this helps somebody.
It brought his to ST attention, and it is still like this, maybe I do something wrong?
I'm mainly using HAL.
I'm also not sure why they removed __FILE__, __LINE__ from the Error_Handler. How would that benefit?
I hope the suggestions will finally make it o the ST developers in charge. But...
The complete sdmmc.c file, unmodified looks like:
/**
******************************************************************************
* File Name : SDMMC.c
* Description : This file provides code for the configuration
* of the SDMMC instances.
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2020 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "sdmmc.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
SD_HandleTypeDef hsd1;
/* SDMMC1 init function */
void MX_SDMMC1_SD_Init(void)
{
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_8B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 2;
hsd1.Init.TranceiverPresent = SDMMC_TRANSCEIVER_NOT_PRESENT;
}
void HAL_SD_MspInit(SD_HandleTypeDef* sdHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(sdHandle->Instance==SDMMC1)
{
/* USER CODE BEGIN SDMMC1_MspInit 0 */
/* USER CODE END SDMMC1_MspInit 0 */
/* SDMMC1 clock enable */
__HAL_RCC_SDMMC1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**SDMMC1 GPIO Configuration
PC8 ------> SDMMC1_D0
PC9 ------> SDMMC1_D1
PC10 ------> SDMMC1_D2
PC11 ------> SDMMC1_D3
PC12 ------> SDMMC1_CK
PD2 ------> SDMMC1_CMD
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11
|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* SDMMC1 interrupt Init */
HAL_NVIC_SetPriority(SDMMC1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
/* USER CODE BEGIN SDMMC1_MspInit 1 */
/* USER CODE END SDMMC1_MspInit 1 */
}
}
void HAL_SD_MspDeInit(SD_HandleTypeDef* sdHandle)
{
if(sdHandle->Instance==SDMMC1)
{
/* USER CODE BEGIN SDMMC1_MspDeInit 0 */
/* USER CODE END SDMMC1_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_SDMMC1_CLK_DISABLE();
/**SDMMC1 GPIO Configuration
PC8 ------> SDMMC1_D0
PC9 ------> SDMMC1_D1
PC10 ------> SDMMC1_D2
PC11 ------> SDMMC1_D3
PC12 ------> SDMMC1_CK
PD2 ------> SDMMC1_CMD
*/
HAL_GPIO_DeInit(GPIOC, GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11
|GPIO_PIN_12);
HAL_GPIO_DeInit(GPIOD, GPIO_PIN_2);
/* SDMMC1 interrupt Deinit */
HAL_NVIC_DisableIRQ(SDMMC1_IRQn);
/* USER CODE BEGIN SDMMC1_MspDeInit 1 */
/* USER CODE END SDMMC1_MspDeInit 1 */
}
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2020-05-20 5:26 PM
Super! The EXTCSD registers were not accessed in the past.