2021-08-05 06:45 AM
Hello @Khouloud ZEMMELI
Please refer to attachment.
After I installed and used the latest STM32CubeMX version 6.3.0, I am observing an issue. The PIN names that I had used in the IOC file, are now no longer present as macros in the generated code. Without the macro I no longer know the use of the PIN and have to refer to Schematics. The STM32CubeH7 MCU package version in use is unchanged and is 1.9.0
Please suggest a fix.
Thanks,
Rajeev
2021-08-05 06:52 AM
Hello @Rajeev Arora ,
Could you please share the original ioc file created with the previous version? I need to know some details such as the Part Number used and IPs configured to be able to reproduce the issue..
Thanks, Khouloud
2021-08-05 06:54 AM
Hi,
It appears that under Project Manager -> Advance Settings I had to manually change the settings for GPIO to first HAL, store it and then change it back to LL to get the correct output. I have to do the similar changes for RCC as well. Maybe an issue with the LL selection exists.
Thanks,
Rajeev
2021-08-05 06:58 AM
Hi @Khouloud ZEMMELI
Is there a link where is only visible to me and ST. As the file relates with a product, I will not like to share it here in the community.
Thanks,
Rajeev
2021-08-05 06:59 AM
Sure, you can send me your project in a private message 🙂
Khouloud
2021-08-05 07:57 AM
Hi,
Unable to figure out how to send a private email from ST Community. I would need the details in order to send an email via my official email.
Thanks,
Rajeev
2021-08-09 03:11 AM
Hello @Rajeev Arora
Just put the cursor on my name, then you will find a Message button, as mentioned in the image below, simple click on it, you can send me your project there.
If you still face a problem, don't hesitate to tell me 🙂
Khouloud
2021-08-11 04:15 AM
2021-08-13 01:10 AM
Ok, I'll be waiting for your return 🙂
Khouloud
2021-08-26 05:18 AM
Dear @Khouloud ZEMMELI ,
You may use the IOC file that I shared with a different query.
My observation is that when I am setting RCC and GPIO to use LL drivers, and let the ETHERNET, FDCAN, (some) USARTs still use the HAL drivers, then this issue is observed:
Example: STM32CubeMX is overwriting exiting code:
```
HAL_GPIO_DeInit(GPIOC, ETH_MDC_PC01_Pin|ETH_RXD0_PC04_Pin|ETH_RXD1_PC05_Pin);
HAL_GPIO_DeInit(GPIOA, ETH_REF_CLK_PA01_Pin|ETH_MDIO_PA02_Pin|ETH_CRS_DV_PA07_Pin);
HAL_GPIO_DeInit(GPIOB, ETH_TXD0_PB12_Pin|ETH_TXD1_PB13_Pin);
HAL_GPIO_DeInit(ETH_TX_EN_PG11_GPIO_Port, ETH_TX_EN_PG11_Pin);
```
with:
```
HAL_GPIO_DeInit(GPIOC, GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5);
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_7);
HAL_GPIO_DeInit(GPIOB, GPIO_PIN_12|GPIO_PIN_13);
HAL_GPIO_DeInit(GPIOG, GPIO_PIN_11);
```
This change is of concern to me, as now I do not know what is the use of GPIO_PIN_1. Instead it it would have still read as ETH_MDC_PC01_Pin, the informative name would have been more helpful.
Please help fix the issue.
Thanks,
Rajeev