2023-03-08 6:07 AM - last edited on 2024-05-25 11:07 AM by Tesla DeLorean
Hi there,
I'm trying to use an NHD-2.7-12864WDW3 model OLED LCD that has SSD1322 driver. Im using m68 parallel interface.
The MPU im using is Nucleo-F072RB and im using CUBEMX for adjusting it's settings and using KEIL IDE for coding. Whatever i done i cannot make it work and i don't know what is causing this problem. Can u guys help me pls? Here is my code
This is for functions
void send_to_lcd(char data, int dc)
{
HAL_GPIO_WritePin(D7_GPIO_Port, D7_Pin, ((data>>7)&0x01));
HAL_GPIO_WritePin(D6_GPIO_Port, D6_Pin, ((data>>6)&0x01));
HAL_GPIO_WritePin(D5_GPIO_Port, D5_Pin, ((data>>5)&0x01));
HAL_GPIO_WritePin(D4_GPIO_Port, D4_Pin, ((data>>4)&0x01));
HAL_GPIO_WritePin(D3_GPIO_Port, D3_Pin, ((data>>3)&0x01));
HAL_GPIO_WritePin(D2_GPIO_Port, D2_Pin, ((data>>2)&0x01));
HAL_GPIO_WritePin(D1_GPIO_Port, D1_Pin, ((data>>1)&0x01));
HAL_GPIO_WritePin(D0_GPIO_Port, D0_Pin, ((data>>0)&0x01));
HAL_GPIO_WritePin(DC_GPIO_Port, DC_Pin, dc); // 0 command, 1 data
HAL_GPIO_WritePin(RW_GPIO_Port,RW_Pin,GPIO_PIN_RESET);
HAL_GPIO_WritePin(CS_GPIO_Port,CS_Pin,GPIO_PIN_RESET);
HAL_Delay(1);
HAL_GPIO_WritePin(E_GPIO_Port, E_Pin, GPIO_PIN_SET);
HAL_Delay(1);
HAL_GPIO_WritePin(E_GPIO_Port, E_Pin, GPIO_PIN_RESET);
HAL_Delay(1);
HAL_GPIO_WritePin(CS_GPIO_Port,CS_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(RW_GPIO_Port,RW_Pin,GPIO_PIN_SET);
}
void lcd_send_cmd (char cmd)
{
send_to_lcd(cmd, 0); // 0 COMMAND
}
void lcd_send_data (char data)
{
send_to_lcd(data, 1); // 1 DATA
}
void lcd_send_string (char *str)
{
while(*str) lcd_send_data (*str++);
}
void Set_Column_Address_12864(unsigned char a, unsigned char b)
{
lcd_send_cmd(0x15); // Set Column Address
lcd_send_data(a); // Default => 0x00
lcd_send_data(b); // Default => 0x77
}
void Set_Row_Address_12864(unsigned char a, unsigned char b)
{
lcd_send_cmd(0x75); // Set Row Start and End Address
lcd_send_data(a); // Default => 0x00
lcd_send_data(b); // Default => 0x7F
}
void Set_Write_RAM_12864()
{
lcd_send_cmd(0x5C); // Enable MCU to Write DATA RAM
}
void Set_Read_RAM_12864()
{
lcd_send_cmd(0x5D); // Enable MCU to Read DATA RAM
}
void NHD12864WDY3_Init(void)
{
HAL_GPIO_WritePin(RES_GPIO_Port, RES_Pin, GPIO_PIN_RESET); //pull /RES (pin #16) low
HAL_Delay(1); //keep /RES low for minimum 200µs
HAL_GPIO_WritePin(RES_GPIO_Port, RES_Pin, GPIO_PIN_SET); //pull /RES high
HAL_Delay(1); //wait minimum 200µs before sending commands
lcd_send_cmd(0xAE); //display OFF SLEEP MODE
lcd_send_cmd(0xB3); //set CLK div. & OSC freq.
lcd_send_data(0x91);
lcd_send_cmd(0xCA); //set MUX ratio+
lcd_send_data(0x3F);
lcd_send_cmd(0xA2); //set offset +
lcd_send_data(0x00);
lcd_send_cmd(0xAB); //function selection
lcd_send_data(0x01);
lcd_send_cmd(0xA0); //set re-map
lcd_send_data(0x16);
lcd_send_data(0x11);
lcd_send_cmd(0xC7); //master contrast current+
lcd_send_data(0x0F);
lcd_send_cmd(0xC1); //set contrast current+
lcd_send_data(0x9F);
lcd_send_cmd(0xB1); //set phase length
lcd_send_data(0xF2);
lcd_send_cmd(0xBB); //set pre-charge voltage
lcd_send_data(0x1F);
lcd_send_cmd(0xB4); //set VSL
lcd_send_data(0xA0);
lcd_send_data(0xFD);
lcd_send_cmd(0xBE); //set VCOMH
lcd_send_data(0x04);
lcd_send_cmd(0xA6); //set display mode
lcd_send_cmd(0xAF); //display ON SLEEP MODE
}
void FillPixel_12864()
{
unsigned int i, j;
Set_Column_Address_12864(0x1C,0x5B); //1C & 5B = DISPLAY Start & End address.
Set_Row_Address_12864(0x00,0x3F);
for(i=0;i<32;i++) //Columns
{
for(j=0;j<64;j++) //Rows
{
lcd_send_data(0xFF);
HAL_Delay(1);
lcd_send_data(0x00);
HAL_Delay(1);
}
for(j=0;j<64;j++) //Rows
{
lcd_send_data(0x00);
HAL_Delay(1);
lcd_send_data(0xFF);
HAL_Delay(1);
Set_Write_RAM_12864();
}
}
}
void ClearPixel_12864()
{
unsigned int i, j;
Set_Column_Address_12864(0x1C,0x5B);
Set_Row_Address_12864(0x00,0x3F);
Set_Write_RAM_12864();
for(i=0;i<64;i++) //Columns
{
for(j=0;j<128;j++) //Rows
{
lcd_send_data(0x00);
HAL_Delay(100);
}
}
}
and this is for part of the main.c
HAL_GPIO_WritePin(RES_GPIO_Port, RES_Pin, GPIO_PIN_RESET);
HAL_Delay(1);
HAL_GPIO_WritePin(RES_GPIO_Port, RES_Pin, GPIO_PIN_SET);
HAL_Delay(1);
NHD12864WDY3_Init();
HAL_Delay(1);
while (1)
{
HAL_GPIO_TogglePin (GPIOA, GPIO_PIN_5);
HAL_Delay(200);
Set_Column_Address_12864(0x00, 0x77);
Set_Row_Address_12864(0x00, 0x7F);
lcd_send_string("Hello World");
HAL_Delay(200);
}
and here is the CUBEMX pin I/O's (D11 RES,D12 CS)
i tried to supply it with external voltage 3.3v so i don't think there is any ampere or voltage problem.
The display doesn't show anything when i power it so i don't know what to do
2023-03-08 8:06 AM
Observe using Logic Analyzer, and show us the waveforms on the display's pins.
JW
2023-03-08 10:36 AM
Are there perhaps registers you can read-back and confirm communications?
https://newhavendisplay.com/content/specs/NHD-2.7-12864WDW3.pdf
https://newhavendisplay.com/content/app_notes/SSD1322.pdf
Common grounds? When you used an external 3.3V supply, what kind of current did it draw.
Show wiring to OLED header.
2023-03-09 3:08 AM
yes i plugged them in Breadboard so i think it's common ground The external supply i'm using is voltage regulator STEVAL-ISA156V1. The wiring of the setup is like this
2023-03-09 3:09 AM
sorry i don't have a logic analyser im checking the pins with multimeter
2023-03-09 3:28 AM
And i tried to measure the pin signals but it seems like D0 and D1 pin doesn't work properly. Or it does but im new to stm so i don't know how to use them as output. so i arrange the pins like thisRes pin is at PC8
2024-05-25 9:38 AM
Hi Kannic... is it working? please help me!! I am also trying but something is wrong so display will always in black screen.
2024-05-25 11:14 AM
From your other post.
"Sir, i have some questions. NHD 3.12 25664 and SSD1322 both are same display? actually i am trying on STM32F411 with NHD 3.12. Please help me and guide me!!"
Show your wiring, Show your code. Used some GitHub libraries, state which
Perhaps use the R/W pin to read-back data written so you can verify you have the interface built correctly.