cancel
Showing results for 
Search instead for 
Did you mean: 

How to access mutexes and semaphores generated by STM32CubeIDE FreeRTOS integration from another file?

Dolence
Associate III

I'm using a mutex to share the I2C bus between an OLED display and an EEPROM. I'm using the IDE to generate the FreeRTOS configuration and tasks initialization (freertos.c file). I have an external file where all the LCD writing occurs. How could I access the mutexes handle generated on freertos.c file from this other file?

...
 
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN Variables */
 
/* USER CODE END Variables */
/* Definitions for defaultTask */
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
  .name = "defaultTask",
  .stack_size = 128 * 4,
  .priority = (osPriority_t) osPriorityNormal,
};
/* Definitions for modbusTask */
osThreadId_t modbusTaskHandle;
const osThreadAttr_t modbusTask_attributes = {
  .name = "modbusTask",
  .stack_size = 64 * 4,
  .priority = (osPriority_t) osPriorityNormal,
};
/* Definitions for dispTask */
osThreadId_t dispTaskHandle;
const osThreadAttr_t dispTask_attributes = {
  .name = "dispTask",
  .stack_size = 300 * 4,
  .priority = (osPriority_t) osPriorityLow,
};
/* Definitions for taskButton */
osThreadId_t taskButtonHandle;
const osThreadAttr_t taskButton_attributes = {
  .name = "taskButton",
  .stack_size = 256 * 4,
  .priority = (osPriority_t) osPriorityLow,
};
/* Definitions for i2cmutex */
osMutexId_t i2cmutexHandle;
const osMutexAttr_t i2cmutex_attributes = {
  .name = "i2cmutex"
};
 
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN FunctionPrototypes */
 
/* USER CODE END FunctionPrototypes */
 
void StartDefaultTask(void *argument);
void StartModbus(void *argument);
void StartDisp(void *argument);
void StartTaskButton(void *argument);
 
void MX_FREERTOS_Init(void); /* (MISRA C 2004 rule 8.1) */
 
/* Hook prototypes */
void configureTimerForRunTimeStats(void);
unsigned long getRunTimeCounterValue(void);
void vApplicationStackOverflowHook(xTaskHandle xTask, signed char *pcTaskName);
 
/* USER CODE BEGIN 1 */
/* Functions needed when configGENERATE_RUN_TIME_STATS is on */
__weak void configureTimerForRunTimeStats(void)
{
 
}
 
__weak unsigned long getRunTimeCounterValue(void)
{
return 0;
}
/* USER CODE END 1 */
 
/* USER CODE BEGIN 4 */
void vApplicationStackOverflowHook(xTaskHandle xTask, signed char *pcTaskName)
{
   /* Run time stack overflow checking is performed if
   configCHECK_FOR_STACK_OVERFLOW is defined to 1 or 2. This hook function is
   called if a stack overflow is detected. */
}
/* USER CODE END 4 */
 
/**
  * @brief  FreeRTOS initialization
  * @param  None
  * @retval None
  */
void MX_FREERTOS_Init(void) {
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
  /* Create the mutex(es) */
  /* creation of i2cmutex */
  i2cmutexHandle = osMutexNew(&i2cmutex_attributes);  // <-  I WANT TO ACCESS THIS HANDLER FROM OUTSIDE THIS FILE
 
...

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

From your external file use the storage class extern:

extern osMutexId_t i2cmutexHandle;

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

From your external file use the storage class extern:

extern osMutexId_t i2cmutexHandle;

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.