2022-02-06 07:48 PM
Environment:
tool: STM32CubeMX6.4.0
cpu: STM32H755XI
Repos: STM32Cube_FW_H7_V1.9.1
I configured pins as GPIO input/output by STM32CubeMX GUI. MAX_GPIO_Init() is auto-generated and all pins are configured inside. However it is not called by any function. Usually it will be called in main().
Below is the auto-gernerated main() function code. MAX_GPIO_Init() is missed. Is it a abnormal case?
My ioc file for this case is also attached.
Thanks.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
int32_t timeout;
/* USER CODE END Boot_Mode_Sequence_0 */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* USER CODE BEGIN Boot_Mode_Sequence_1 */
/* Wait until CPU2 boots and enters in stop mode or timeout*/
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
/* USER CODE END Boot_Mode_Sequence_1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
/* USER CODE END Boot_Mode_Sequence_2 */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_DMA_Init();
MX_UART7_Init();
MX_RTC_Init();
MX_MDMA_Init();
MX_QUADSPI_Init();
MX_I2C2_Init();
MX_SDMMC1_MMC_Init();
MX_TIM5_Init();
MX_UART8_Init();
MX_DAC1_Init();
MX_SAI1_Init();
MX_SPI4_Init();
MX_SPI5_Init();
MX_UART4_Init();
MX_RNG_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Init scheduler */
osKernelInitialize(); /* Call init function for freertos objects (in freertos.c) */
MX_FREERTOS_Init();
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2022-02-08 03:00 AM
Hello @Lzhou.1 ,
Thanks for your feedback,
It seems that you checked the " Do not Generate Function Call " in your CubeMX configuration.
Could you please uncheck it and check the visibility field instead, just like the attachment below.
I hope this helps !
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly
Sara.
2022-02-08 03:00 AM
Hello @Lzhou.1 ,
Thanks for your feedback,
It seems that you checked the " Do not Generate Function Call " in your CubeMX configuration.
Could you please uncheck it and check the visibility field instead, just like the attachment below.
I hope this helps !
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly
Sara.
2022-02-08 08:37 PM
Yes, it works, thank you very much!