2015-06-19 07:17 PM
What is the meaning of IP in the STM32CubeMX software? I looked at the documentation, but I don�t find it and google obviously show me TCP/IP. Thank you.
#cube #stm32cubemx2015-06-19 08:00 PM
Intellectual Property? Stuff covered by Copyrights, Patents, or Trade Secrets
2015-06-19 08:48 PM
Well, in IP menu appears: ADC1, ADC2, ADC3, CAN1, CAN2, CRC, DAC, DCMI, ETH... etc. So I don´t think it means Intellectual Property.
2015-06-20 12:11 AM
IP refers to peripherals, in that context.
See Wikipedia:https://en.wikipedia.org/wiki/Semiconductor_intellectual_property_core
2015-06-20 11:54 AM
Thank you. It is clear now.
2015-06-23 05:33 AM
Hi Vinicio,
I confirm what was said by jb.But as I see with CubeMX 4.8, I think that it was replaced by correct word (Peripheral). Is there any location where ''IP'' is still being used?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-06-25 09:35 AM
Hello Mayla. I just realized that I am using version 4.2.0. I am going to update to 4.8.0 today!
Thank you.2024-03-12 02:07 PM
"Add IP Handle Label"