cancel
Showing results for 
Search instead for 
Did you mean: 

Meaning of IP in STM32CubeMX

vinicio
Associate II
Posted on June 20, 2015 at 04:17

What is the meaning of IP in the STM32CubeMX software? I looked at the documentation, but I don�t find it and google obviously show me TCP/IP. Thank you.

#cube #stm32cubemx
7 REPLIES 7
Posted on June 20, 2015 at 05:00

Intellectual Property? Stuff covered by Copyrights, Patents, or Trade Secrets

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
vinicio
Associate II
Posted on June 20, 2015 at 05:48

Well, in IP menu appears: ADC1, ADC2, ADC3, CAN1, CAN2, CRC, DAC, DCMI, ETH... etc. So I don´t  think it means Intellectual Property.

james2399
Associate II
Posted on June 20, 2015 at 09:11

IP refers to peripherals, in that context.

See Wikipedia: 

https://en.wikipedia.org/wiki/Semiconductor_intellectual_property_core

vinicio
Associate II
Posted on June 20, 2015 at 20:54

Thank you. It is clear now. 

Amel NASRI
ST Employee
Posted on June 23, 2015 at 14:33

Hi Vinicio,

I confirm what was said by jb.

But as I see with CubeMX 4.8, I think that it was replaced by correct word (Peripheral). Is there any location where ''IP'' is still being used?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

vinicio
Associate II
Posted on June 25, 2015 at 18:35

Hello Mayla. I just realized that I am using version 4.2.0. I am going to update to 4.8.0 today!

Thank you.

KevinWoo_0-1710277604747.png

"Add IP Handle Label"